imx7d can't enter mfg download mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7d can't enter mfg download mode

Jump to solution
1,048 Views
yan2anfei
Contributor III

hi,

I have a imx7dsabre board.

I set the BOOTMODE=01  MFG mode.

boot form sd 00100000.

the system can't enter usb download mode, but if I take out the sd card ,the mfg software can find my imx7dsabre board. then I insert the sd card,the usb download program works well.

my imx6slevk board set different mode is works well. Whether the imx7dsabre board has some problem.

Thanks & Best Regards!

Labels (1)
0 Kudos
1 Solution
727 Views
igorpadykov
NXP Employee
NXP Employee

Hi yan2

behaviour may be caused by SD/MMC Manufacture Mode, from

sect.6.6.12 SD/MMC Manufacture Mode i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

"..boot will go to SD/MMC manufacture mode before serial download mode..

By default, SD/MMC manufacture mode is enabled

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

5 Replies
728 Views
igorpadykov
NXP Employee
NXP Employee

Hi yan2

behaviour may be caused by SD/MMC Manufacture Mode, from

sect.6.6.12 SD/MMC Manufacture Mode i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

"..boot will go to SD/MMC manufacture mode before serial download mode..

By default, SD/MMC manufacture mode is enabled

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

727 Views
yan2anfei
Contributor III

hi igor,

thanks for you reply. I need to  blow the fuse of DISABLE_SDMMC_MFG.

but I can't find the method about how to blow the efuse.

The cmd of imxotp  is not exist in  my uboot cmd.

Can you give me some help? 

Thanks & Best Regards

yan2anfei

0 Kudos
727 Views
igorpadykov
NXP Employee
NXP Employee

please try

http://boundarydevices.com/fuse-command/

Best regards
igor

727 Views
yan2anfei
Contributor III

hi igor,

thanks for you reply.

I wan't to disable  SDMMC_MFG mode.

I use the fuse cmd of uboot.

but I can't find the bit of DISABLE_SDMMC_MFG  from OTP bank0 to bank16.

Best regards
yan2anfei

0 Kudos
727 Views
igorpadykov
NXP Employee
NXP Employee

please check Table 6-17. Boot Fusemap i.MX7D RM p.1055

fuse Disable SDMMC Manufacture mode

Best regards
igor

0 Kudos