Dear support,
I am working with a imx6ull evk where we mount a NAND flash Micron 29F4G08ABADA .
I setup the resistor like the volansys gateway that use Micron 29F8G8ABABA and imx6ul.
Now using mfgtool L4.9.11_1.0.0-ga_mfg-tools I have the error that the kernel is unable to erase /dev/mtd0 0 0 .
I read that in the mfg tools L4.1.15_2.0.0-ga_mfg-tools it was required a kernel mods and recompile in order to add the GPMI driver in the kernel used to boot the board via usb.
Is it true even with the L4.9.11 that the kernel mod is required?
Do I need to recompile the kernel adding the gpmi driver?
Thanks in advance,
Stefano.
Hi stefano
manufacturing tool kernel is built using the imx_v7_mfg_defconfig
as described in sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide
and it includes gpmi nand driver
imx_v7_mfg_defconfig\configs\arm\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
thank you for your prompt reply.
I apologize for the long post, but I am unable to find how to attach a file in the reply.
So could it be the wrong resistor layout?
Here you can find a picture of my module.
In the mfg-tool I am running the mfgtool2-yocto-mx-evk-nand.vbs and here you can find the log:
U-Boot 2017.03-imx_v2017.03_4.9.11_1.0.0_ga+ga2fea67 (Sep 17 2017 - 15:09:34 -0500) CPU: Freescale i.MX6ULL rev1.0 528 MHz (running at 396 MHz) CPU: Commercial temperature grade (0C to 95C) at 42C Reset cause: POR Model: Freescale i.MX6 ULL 14x14 EVK Board Board: MX6ULL 14x14 EVK DRAM: 512 MiB NAND: 0 MiB MMC: FSL_SDHC: 0 *** Warning - readenv() failed, using default environment Display: TFT43AB (480x272) Video: 480x272x24 In: serial Out: serial Err: serial Net: Warning: ethernet@020b4000 using MAC address from ROM eth1: ethernet@020b4000 [PRIME] Warning: ethernet@02188000 using MAC address from ROM , eth0: ethernet@02188000 Boot from USB for mfgtools Use default environment for mfgtools Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; Hit any key to stop autoboot: 0 Kernel image @ 0x80800000 [ 0x000000 - 0x5bd9c8 ] ## Loading init Ramdisk from Legacy Image at 83800000 ... Image Name: fsl-image-mfgtool-initramfs-imx6 Image Type: ARM Linux RAMDisk Image (gzip compressed) Data Size: 8594034 Bytes = 8.2 MiB Load Address: 00000000 Entry Point: 00000000 Verifying Checksum ... OK ## Flattened Device Tree blob at 83000000 Booting using the fdt blob at 0x83000000 Using Device Tree in place at 83000000, end 8300bf4c Modify /soc/aips-bus@02200000/epdc@0228c000:status disabled ft_system_setup for mx6 Starting kernel ... Booting Linux on physical CPU 0x0 Linux version 4.9.11+ (bamboo@yb4) (gcc version 6.2.0 (GCC) ) #1 SMP PREEMPT Sun Sep 17 14:25:24 CDT 2017 CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d CPU: div instructions available: patching division code CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache OF: fdt:Machine model: Freescale i.MX6 ULL 14x14 EVK Board Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool Memory policy: Data cache writealloc percpu: Embedded 14 pages/cpu @8bb31000 s25740 r8192 d23412 u57344 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048 Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= mtdparts=gpmi-nand:64m(boot),16m(kernel),16m(dtb),1m(misc),-(rootfs) clk_ignore_unused PID hash table entries: 2048 (order: 1, 8192 bytes) Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) Memory: 170800K/524288K available (7168K kernel code, 330K rwdata, 2624K rodata, 1024K init, 441K bss, 25808K reserved, 327680K cma-reserved, 0K highmem) Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xffc00000 - 0xfff00000 (3072 kB) vmalloc : 0xa0800000 - 0xff800000 (1520 MB) lowmem : 0x80000000 - 0xa0000000 ( 512 MB) pkmap : 0x7fe00000 - 0x80000000 ( 2 MB) modules : 0x7f000000 - 0x7fe00000 ( 14 MB) .text : 0x80008000 - 0x80800000 (8160 kB) .init : 0x80b00000 - 0x80c00000 (1024 kB) .data : 0x80c00000 - 0x80c52820 ( 331 kB) .bss : 0x80c54000 - 0x80cc26dc ( 442 kB) SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Preemptible hierarchical RCU implementation. Build-time adjustment of leaf fanout to 32. RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1. RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1 NR_IRQS:16 nr_irqs:16 16 Switching to timer-based delay loop, resolution 333ns sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns Console: colour dummy device 80x30 Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) CPU: Testing write buffer coherency: ok /cpus/cpu@0 missing clock-frequency property CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 Setting up static identity map for 0x80100000 - 0x80100070 Brought up 1 CPUs SMP: Total of 1 processors activated (6.00 BogoMIPS). CPU: All CPU(s) started in SVC mode. devtmpfs: initialized VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns pinctrl core: initialized pinctrl subsystem NET: Registered protocol family 16 DMA: preallocated 256 KiB pool for atomic coherent allocations cpuidle: using governor menu hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. hw-breakpoint: maximum watchpoint size is 8 bytes. imx6ul-pinctrl 20e0000.iomuxc: no fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6ull-evk-gpmi-rework imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver imx6ul-pinctrl 2290000.iomuxc-snvs: initialized IMX pinctrl driver mxs-dma 1804000.dma-apbh: initialized SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb i2c i2c-0: IMX I2C adapter registered i2c i2c-0: can't use DMA, using PIO instead. i2c i2c-1: IMX I2C adapter registered i2c i2c-1: can't use DMA, using PIO instead. Linux video capture interface: v2.00 pps_core: LinuxPPS API ver. 1 registered pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> PTP clock support registered imx rpmsg driver is registered. Advanced Linux Sound Architecture Driver Initialized. clocksource: Switched to clocksource mxc_timer1 VFS: Disk quotas dquot_6.6.0 VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) NET: Registered protocol family 2 TCP established hash table entries: 4096 (order: 2, 16384 bytes) TCP bind hash table entries: 4096 (order: 3, 32768 bytes) TCP: Hash tables configured (established 4096 bind 4096) UDP hash table entries: 256 (order: 1, 8192 bytes) UDP-Lite hash table entries: 256 (order: 1, 8192 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. Trying to unpack rootfs image as initramfs... Freeing initrd memory: 8396K (83800000 - 84033000) Bus freq driver module loaded futex hash table entries: 256 (order: 2, 16384 bytes) workingset: timestamp_bits=30 max_order=17 bucket_order=0 NFS: Registering the id_resolver key type Key type id_resolver registered Key type id_legacy registered jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. fuse init (API version 7.26) io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) imx-weim 21b8000.weim: Driver registered. backlight supply power not found, using dummy regulator 21c8000.lcdif supply lcd not found, using dummy regulator mxsfb 21c8000.lcdif: failed to find mxc display driver Console: switching to colour frame buffer device 60x34 mxsfb 21c8000.lcdif: initialized imx-sdma 20ec000.sdma: loaded firmware 3.3 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a IMX random: fast init done console [ttymxc0] enabled 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 72, base_baud = 5000000) is a IMX imx sema4 driver is registered. [drm] Initialized [drm] Initialized vivante 1.0.0 20120216 on minor 0 brd: module loaded loop: module loaded imx6ul-pinctrl 20e0000.iomuxc: unable to find group for node gpmi-nand-1 gpmi-nand: probe of 1806000.gpmi-nand failed with error -22 libphy: Fixed MDIO Bus: probed 20b4000.ethernet supply phy not found, using dummy regulator pps pps0: new PPS source ptp0 libphy: fec_enet_mii_bus: probed fec 20b4000.ethernet eth0: registered PHC device 0 2188000.ethernet supply phy not found, using dummy regulator pps pps1: new PPS source ptp1 fec 2188000.ethernet eth1: registered PHC device 1 ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver ehci-mxc: Freescale On-Chip EHCI Host driver usbcore: registered new interface driver usb-storage 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator 2184000.usb supply vbus not found, using dummy regulator 2184200.usb supply vbus not found, using dummy regulator ci_hdrc ci_hdrc.1: EHCI Host Controller ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1 ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected Mass Storage Function, version: 2009/09/11 LUN: removable file: (no medium) LUN: removable read only file: /fat Number of LUNs=1 g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11 g_mass_storage gadget: g_mass_storage ready mousedev: PS/2 mouse device common for all mice input: 20cc000.snvs:snvs-powerkey as /devices/soc0/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0 input: iMX6UL Touchscreen Controller as /devices/soc0/soc/2000000.aips-bus/2040000.tsc/input/input1 snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0 i2c /dev entries driver IR NEC protocol handler initialized IR RC5(x/sz) protocol handler initialized IR RC6 protocol handler initialized IR JVC protocol handler initialized IR Sony protocol handler initialized IR SANYO protocol handler initialized IR Sharp protocol handler initialized IR MCE Keyboard/mouse protocol handler initialized IR XMP protocol handler initialized pxp-v4l2 pxp_v4l2: initialized imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0) sdhci: Secure Digital Host Controller Interface driver sdhci: Copyright(c) Pierre Ossman sdhci-pltfm: SDHCI platform and OF driver helper sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA usbcore: registered new interface driver usbhid usbhid: USB HID core driver NET: Registered protocol family 10 sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage NET: Registered protocol family 17 Key type dns_resolver registered cpu cpu0: Registered imx6q-cpufreq Registering SWP/SWPB emulation handler imx_thermal 2000000.aips-bus:tempmon: Commercial CPU temperature grade - max:95C critical:90C passive:85C snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:01:33 UTC (93) clk: Not disabling unused clocks can-3v3: disabling gpio_dvfs: disabling ALSA device list: No soundcards found. Freeing unused kernel memory: 1024K (80b00000 - 80c00000) Mass Storage Function, version: 2009/09/11 LUN: removable file: (no medium) MFG tool will use 1st udc:ci_hdrc.0 /linuxrc: line 37: echo: write error: Device or resource busy Starting UTP uuc 0.5 [built Sep 15 2017 15:12:19] UTP: Waiting for device to appear UTP: file/device node /dev/utp already exists cpu_id is 0 UTP: received command '$ mount -t debugfs debugfs /sys/kernel/debug' UTP: executing "mount -t debugfs debugfs /sys/kernel/debug" UTP: sending Success to kernel for command $ mount -t debugfs debugfs /sys/kernel/debug. utp_poll: pass returned. UTP: received command '$ flash_erase /dev/mtd0 0 0' UTP: executing "flash_erase /dev/mtd0 0 0" flash_erase: error!: /dev/mtd0 error 2 (No such file or directory) UTP: sending Non-success to kernel for command $ flash_erase /dev/mtd0 0 0. utp_poll: exit with status 65280
The last part of the log is quite clear, the kernel can't see the /dev/mtd0 device.
The flash is brand new, so I suppose that is not formatted, but I don't know how to do this.
I want to remark the flash part number Micron 29F4G08ABADA.
Thank you for your help.
Best regards,
Stefano.
Hi Stefano
one can check mx6ul_14x14_evk_nand_defconfig from
How-To use NAND boot on i.MX6UL EVK board
https://community.nxp.com/thread/453809
Best regards
igor