How to test USB2514i (hub) eye diagram in imx6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to test USB2514i (hub) eye diagram in imx6Q

1,028件の閲覧回数
zohanlin
Contributor IV

Dear all,

I want to test the USB2514i eye diagram in imx6Q, and it is connected to USB HOST.

I use the command as below :

memtool -32 0x020c4080=0x3

memtool -32 0x02184340=0x2
memtool -32 0x02184384=0x1C040000

I can detect the signal between CPU and HUB, but I can't detect anything between HUB and miniPCIe.

Could anyone tell me how to solve the problem?

Thanks,

zohan

ラベル(3)
0 件の賞賛
返信
1 返信

958件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zohan

from i.MX6Q usb side one can try to follow procedure described on

I.MX6 series USB Certification Guides 

for USB2514i eye diagram may be suggested to apply to vendor of that chip Home | Microchip Technology 

http://ww1.microchip.com/downloads/jp/DeviceDoc/jp567224.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信