imx6ull bitbake qt3d failed with latest yocto 6.6.3 BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull bitbake qt3d failed with latest yocto 6.6.3 BSP

Jump to solution
1,484 Views
Nobita
Contributor III

Hello Sir,

    I have tested build latest yocto 6.6.3 BSP for imx6ullevk board, here are my steps:

 

repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-nanbield -m imx-6.6.3-1.0.0.xml

repo sync

DISTRO=fsl-imx-xwayland MACHINE=imx6ull14x14evk  source imx-setup-release.sh -b imx6ullevk-xwayland

bitbake -k imx-image-full

bitbake -k imx-image-full -c populate_sdk

 

When I tried to bitbake -k imx-image-full -c populate_sdk, I encounter some bitbake fails like bellow:

ERROR: Task (/home/researcher01/workspace/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qtdatavis3d_git.bb:do_install) failed with exit code '1'
ERROR: Task (/home/researcher01/workspace/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qt3d_git.bb:do_install) failed with exit code '1'

The 2 fail courses are same:

Change Dir: '/home/researcher01/workspace/imx-yocto-bsp/imx6ullevk-xwayland/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/qt3d/6.5.3/build'
|
| Run Build Command(s): ninja -v -j 16 install
| ninja: error: unknown target 'install'


| Change Dir: '/home/researcher01/workspace/imx-yocto-bsp/imx6ullevk-xwayland/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/qtdatavis3d/6.5.3/build'
|
| Run Build Command(s): ninja -v -j 16 install
| ninja: error: unknown target 'install'

So I tried to bitbake them alternatively to see what happend, and I found the question:

bitbake -k qt3d -c devshell
cd ../build
cmake ../git/
Skipping the build as the condition "QT_FEATURE_opengl AND NOT WASM" is not met.
-- Configuring done (1.2s)
-- Generating done (0.0s)
-- Build files have been written to: /home/researcher01/workspace/imx-yocto-bsp/imx6ullevk-xwayland/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/qt3d/6.5.3/build
bitbake -k qtdatavis3d -c devshell
cd ../build
cmake ../git/
-- Could NOT find Qt6OpenGL (missing: Qt6OpenGL_DIR)
CMake Warning at /home/researcher01/workspace/imx-yocto-bsp/imx6ullevk-xwayland/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/qtdatavis3d/6.5.3/recipe-sysroot/usr/lib/cmake/Qt6/Qt6Config.cmake:224 (message):
  Failed to find optional Qt component "OpenGL".

  Expected Config file at
  "/home/researcher01/workspace/imx-yocto-bsp/imx6ullevk-xwayland/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/qtdatavis3d/6.5.3/recipe-sysroot/usr/lib/cmake/Qt6OpenGL/Qt6OpenGLConfig.cmake"
  does NOT exist

Call Stack (most recent call first):
  CMakeLists.txt:15 (find_package)


Skipping the build as the condition "TARGET Qt::OpenGL" is not met.
-- Configuring done (1.2s)
-- Generating done (0.0s)
-- Build files have been written to: /home/researcher01/workspace/imx-yocto-bsp/imx6ullevk-xwayland/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/qtdatavis3d/6.5.3/build

Both of these 2 receipes are not configured properly, However when I tried bitbake another board imx93-11x11-evk with the same bsp, these 2 receipes bitbake workflow works well and do not have the error above, I think there must be some missing configuration should be added to imx6ull bitbake workflow as imx93 does, I have been looking insight for days, comparing meta-imx and meta-freescale codebase, however I did not find any clear clue, please help!

Best Regards!

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,407 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @2458332461 

You can remove these packages in sdk and image. They require opengl.

IMAGE_INSTALL:remove = "qt3d"
TOOLCHAIN_TARGET_TASK:remove = "qt3d"

 

View solution in original post

0 Kudos
Reply
14 Replies
1,462 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Nobita 

This could relate to this flag, as i.MX93 has g2d, so 'no-opengl' flag will work. You can try to add it in PACKAGECONFIG_PLATFORM = ""

Zhiming_Liu_0-1715942714939.png

 

0 Kudos
Reply
1,417 Views
2458332461
Contributor I

Hello Sir,

Following your method of modification, this error still exists.

dc210c23e567a2d378f38554f01d5ee.png

0 Kudos
Reply
1,408 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @2458332461 

You can remove these packages in sdk and image. They require opengl.

IMAGE_INSTALL:remove = "qt3d"
TOOLCHAIN_TARGET_TASK:remove = "qt3d"

 

0 Kudos
Reply
1,229 Views
2458332461
Contributor I

Hi @zhimingqiu 

I tried to do this but still got the same error generating the sdk phase.I think that approach is wrong, Two FAE in China also encountered the same problem

 
 

 

 

0 Kudos
Reply
1,227 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

If you are using i.MX93, you need modify below file

Zhiming_Liu_0-1718186270622.png

The same issue about other i.MX product which doesn't support opengl will be fixed in next BSP.

 

0 Kudos
Reply
1,185 Views
2458332461
Contributor I

Hi  @Zhiming_Liu 
As you mentioned, I made the changes according to the picture, but when I executed the command "bitbake -k imx-image-full -c populate_sdk" or "bitbake -k imx-image-full", the error in the following picture would appear. Even using "bitbake-c cleanall qtdeclarative" does not resolve the error.

 

2458332461_0-1718243431607.png

 

0 Kudos
Reply
1,182 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The previous patch is only for i.MX93. L6.6.23 will fix this issue for all platforms.

For i.MX6ULL and other, need patch again. Please replace meta-imx-sdk/conf/distro/include/fsl-imx-base.inc with below content directly. Then reserve DISTRO_VERSION, this DISTRO_VERSION is for L6.6.23.

 

require conf/distro/poky.conf

DISTRO = "imx-nxp"
DISTRO_NAME = "NXP i.MX Release Distro"
DISTRO_VERSION = "6.6-scarthgap"
DISTROOVERRIDES = "fsl"

MAINTAINER = "NXP <lauren.post@nxp.com>"

POKY_DEFAULT_DISTRO_FEATURES:remove = "${POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE}"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE             ?= "wayland"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE:mx6-nxp-bsp ?= "wayland vulkan"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE:mx7-nxp-bsp ?= "wayland vulkan"
DISTRO_FEATURES:remove = "pulseaudio"

POKY_DEFAULT_DISTRO_FEATURES:append = " ${POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND}"
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND             ?= "jailhouse"
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND:mx6-nxp-bsp ?= ""
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND:mx7-nxp-bsp ?= ""

DISTRO_FEATURES:append:mx8-nxp-bsp = " virtualization"
SKIP_META_VIRT_SANITY_CHECK = "1"

SKIP_META_SECURITY_SANITY_CHECK = "1"
SKIP_META_TPM_SANITY_CHECK = "1"

# Set a more generic tuning for code reuse across parts
DEFAULTTUNE:mx8-nxp-bsp    ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8m-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8qm-nxp-bsp  ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8x-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8ulp-nxp-bsp ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx9-nxp-bsp    ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx91-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx93-nxp-bsp   ?= "armv8a-crc-crypto"

PACKAGECONFIG:append:pn-gstreamer1.0-plugins-ugly = " x264"

PACKAGECONFIG:append:pn-pulseaudio = " autospawn-for-root"

PACKAGECONFIG:append:class-target:pn-qtquick3d     = " examples"
PACKAGECONFIG:append:class-target:pn-qtwebengine   = " examples"

PACKAGECONFIG:append:pn-systemd = " unmanaged-network"

PACKAGECONFIG:append:pn-qtbase = \
    "${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '${PACKAGECONFIG_QTBASE_WAYLAND_APPEND}', '', d)}"
PACKAGECONFIG:remove:pn-qtbase = \
    "${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '${PACKAGECONFIG_QTBASE_WAYLAND_REMOVE}', '', d)}"
PACKAGECONFIG_QTBASE_WAYLAND_APPEND             = ""
PACKAGECONFIG_QTBASE_WAYLAND_REMOVE             = ""
PACKAGECONFIG_QTBASE_WAYLAND_APPEND:imx-nxp-bsp = " gles2 eglfs"
PACKAGECONFIG_QTBASE_WAYLAND_REMOVE:imx-nxp-bsp = "no-opengl linuxfb'"
PACKAGECONFIG_QTBASE_WAYLAND_APPEND:imxgpu      = ""
PACKAGECONFIG_QTBASE_WAYLAND_REMOVE:imxgpu      = ""

PACKAGECONFIG_GRAPHICS:remove:pn-qtbase = \
    "${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '${PACKAGECONFIG_GRAPHICS_QTBASE_WAYLAND_REMOVE}', '', d)}"
PACKAGECONFIG_GRAPHICS_QTBASE_WAYLAND_REMOVE             = ""
PACKAGECONFIG_GRAPHICS_QTBASE_WAYLAND_REMOVE:imx-nxp-bsp = "gl"
PACKAGECONFIG_GRAPHICS_QTBASE_WAYLAND_REMOVE:imxgpu      = ""

 

 

0 Kudos
Reply
1,148 Views
2458332461
Contributor I

Hi @Zhiming_Liu 

As you mentioned, I made the changes according to the picture, but when I executed the command "bitbake -k imx-image-full -c populate_sdk" 、 "bitbake -k imx-image-full"  

ERROR: Task (/home/zmj/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qtdatavis3d_git.bb:do_install) failed with exit code '1'

ERROR: Task (/home/zmj/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qt3d_git.bb:do_install) failed with exit code '1'

2458332461_0-1718268216426.png

zmj@ubuntu:~/imx-yocto-bsp/sources/meta-imx/meta-imx-sdk/conf/distro/include$ cat fsl-imx-base.inc_cp 
require conf/distro/poky.conf

DISTRO = "imx-nxp"
DISTRO_NAME = "NXP i.MX Release Distro"
DISTRO_VERSION = "6.6-nanbield"
DISTROOVERRIDES = "fsl"

MAINTAINER = "NXP <lauren.post@nxp.com>"

POKY_DEFAULT_DISTRO_FEATURES:remove = "${POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE}"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE             ?= "wayland"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE:mx6-nxp-bsp ?= "wayland vulkan"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE:mx7-nxp-bsp ?= "wayland vulkan"
DISTRO_FEATURES:remove = "pulseaudio"

POKY_DEFAULT_DISTRO_FEATURES:append = " ${POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND}"
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND             ?= "jailhouse"
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND:mx6-nxp-bsp ?= ""
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND:mx7-nxp-bsp ?= ""

DISTRO_FEATURES:append:mx8-nxp-bsp = " virtualization"
SKIP_META_VIRT_SANITY_CHECK = "1"

SKIP_META_SECURITY_SANITY_CHECK = "1"
SKIP_META_TPM_SANITY_CHECK = "1"

# Set a more generic tuning for code reuse across parts
DEFAULTTUNE:mx8-nxp-bsp    ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8m-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8qm-nxp-bsp  ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8x-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8ulp-nxp-bsp ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx9-nxp-bsp    ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx91p-nxp-bsp  ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx93-nxp-bsp   ?= "armv8a-crc-crypto"

PACKAGECONFIG:append:pn-gstreamer1.0-plugins-ugly = " x264"

PACKAGECONFIG:append:pn-pulseaudio = " autospawn-for-root"

PACKAGECONFIG:append:class-target:pn-qtquick3d     = " examples"
PACKAGECONFIG:append:class-target:pn-qtwebengine   = " examples"

PACKAGECONFIG:append:pn-systemd = " unmanaged-network"

PACKAGECONFIG:append:mx93-nxp-bsp:pn-qtbase = " gles2"
PACKAGECONFIG:remove:mx93-nxp-bsp:pn-qtbase = "no-opengl linuxfb"
zmj@ubuntu:~/imx-yocto-bsp/sources/meta-imx/meta-imx-sdk/conf/distro/include$ cat fsl-imx-base.inc
require conf/distro/poky.conf

DISTRO = "imx-nxp"
DISTRO_NAME = "NXP i.MX Release Distro"
DISTRO_VERSION = "6.6-nanbield"
DISTROOVERRIDES = "fsl"

MAINTAINER = "NXP <lauren.post@nxp.com>"

POKY_DEFAULT_DISTRO_FEATURES:remove = "${POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE}"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE             ?= "wayland"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE:mx6-nxp-bsp ?= "wayland vulkan"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE:mx7-nxp-bsp ?= "wayland vulkan"
DISTRO_FEATURES:remove = "pulseaudio"

POKY_DEFAULT_DISTRO_FEATURES:append = " ${POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND}"
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND             ?= "jailhouse"
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND:mx6-nxp-bsp ?= ""
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND:mx7-nxp-bsp ?= ""

DISTRO_FEATURES:append:mx8-nxp-bsp = " virtualization"
SKIP_META_VIRT_SANITY_CHECK = "1"

SKIP_META_SECURITY_SANITY_CHECK = "1"
SKIP_META_TPM_SANITY_CHECK = "1"

# Set a more generic tuning for code reuse across parts
DEFAULTTUNE:mx8-nxp-bsp    ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8m-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8qm-nxp-bsp  ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8x-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8ulp-nxp-bsp ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx9-nxp-bsp    ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx91-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx93-nxp-bsp   ?= "armv8a-crc-crypto"

PACKAGECONFIG:append:pn-gstreamer1.0-plugins-ugly = " x264"

PACKAGECONFIG:append:pn-pulseaudio = " autospawn-for-root"

PACKAGECONFIG:append:class-target:pn-qtquick3d     = " examples"
PACKAGECONFIG:append:class-target:pn-qtwebengine   = " examples"

PACKAGECONFIG:append:pn-systemd = " unmanaged-network"

PACKAGECONFIG:append:pn-qtbase = \
    "${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '${PACKAGECONFIG_QTBASE_WAYLAND_APPEND}', '', d)}"
PACKAGECONFIG:remove:pn-qtbase = \
    "${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '${PACKAGECONFIG_QTBASE_WAYLAND_REMOVE}', '', d)}"
PACKAGECONFIG_QTBASE_WAYLAND_APPEND             = ""
PACKAGECONFIG_QTBASE_WAYLAND_REMOVE             = ""
PACKAGECONFIG_QTBASE_WAYLAND_APPEND:imx-nxp-bsp = " gles2 eglfs"
PACKAGECONFIG_QTBASE_WAYLAND_REMOVE:imx-nxp-bsp = "no-opengl linuxfb'"
PACKAGECONFIG_QTBASE_WAYLAND_APPEND:imxgpu      = ""
PACKAGECONFIG_QTBASE_WAYLAND_REMOVE:imxgpu      = ""

PACKAGECONFIG_GRAPHICS:remove:pn-qtbase = \
    "${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '${PACKAGECONFIG_GRAPHICS_QTBASE_WAYLAND_REMOVE}', '', d)}"
PACKAGECONFIG_GRAPHICS_QTBASE_WAYLAND_REMOVE             = ""
PACKAGECONFIG_GRAPHICS_QTBASE_WAYLAND_REMOVE:imx-nxp-bsp = "gl"
PACKAGECONFIG_GRAPHICS_QTBASE_WAYLAND_REMOVE:imxgpu      = ""
repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-nanbield -m imx-6.6.3-1.0.0.xml

repo  sync

DISTRO=fsl-imx-fb MACHINE=imx6ull14x14evk  source imx-setup-release.sh -b imx-yocto-bsp

bitbake  -k imx-image-full  -c populate_sdk

 

0 Kudos
Reply
1,131 Views
2458332461
Contributor I

Hi @Zhiming_Liu 

Excuse me, is there any way to solve this problem, now the project needs to use Qt, but now linux6.6.3 can not get Qt cross-compilation chain.

0 Kudos
Reply
1,109 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Temporary solutions for imx6 without GPU

require conf/distro/poky.conf

DISTRO = "imx-nxp"
DISTRO_NAME = "NXP i.MX Release Distro"
DISTRO_VERSION = "6.6-nanbield"
DISTROOVERRIDES = "fsl"

MAINTAINER = "NXP <lauren.post@nxp.com>"

POKY_DEFAULT_DISTRO_FEATURES:remove = "${POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE}"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE             ?= "wayland"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE:mx6-nxp-bsp ?= "wayland vulkan"
POKY_DEFAULT_DISTRO_FEATURES_IMX_REMOVE:mx7-nxp-bsp ?= "wayland vulkan"
DISTRO_FEATURES:remove = "pulseaudio"

POKY_DEFAULT_DISTRO_FEATURES:append = " ${POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND}"
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND             ?= "jailhouse"
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND:mx6-nxp-bsp ?= ""
POKY_DEFAULT_DISTRO_FEATURES_IMX_APPEND:mx7-nxp-bsp ?= ""

DISTRO_FEATURES:append:mx8-nxp-bsp = " virtualization"
SKIP_META_VIRT_SANITY_CHECK = "1"

SKIP_META_SECURITY_SANITY_CHECK = "1"
SKIP_META_TPM_SANITY_CHECK = "1"

# Set a more generic tuning for code reuse across parts
DEFAULTTUNE:mx8-nxp-bsp    ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8m-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8qm-nxp-bsp  ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8x-nxp-bsp   ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx8ulp-nxp-bsp ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx9-nxp-bsp    ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx91p-nxp-bsp  ?= "armv8a-crc-crypto"
DEFAULTTUNE:mx93-nxp-bsp   ?= "armv8a-crc-crypto"

PACKAGECONFIG:append:pn-gstreamer1.0-plugins-ugly = " x264"

PACKAGECONFIG:append:pn-pulseaudio = " autospawn-for-root"

PACKAGECONFIG:append:class-target:pn-qtquick3d     = " examples"
PACKAGECONFIG:append:class-target:pn-qtwebengine   = " examples"

PACKAGECONFIG:append:pn-systemd = " unmanaged-network"


PACKAGECONFIG:append:mx93-nxp-bsp:pn-qtbase = " gles2"
PACKAGECONFIG:remove:mx93-nxp-bsp:pn-qtbase = "no-opengl linuxfb"

PACKAGECONFIG:append:mx6-nxp-bsp:pn-qtbase = " gles2"
PACKAGECONFIG:remove:mx6-nxp-bsp:pn-qtbase = "no-opengl linuxfb"

 

0 Kudos
Reply
995 Views
2458332461
Contributor I

Hi @Zhiming_Liu 

Thank you very much for your reply. Is there any way not to shut down GPU? In product use, we need to use GPU to reduce the problem of high CPU usage caused by Qt program.

0 Kudos
Reply
984 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

i.MX6ULL doesn't have GPU, for other imx6 chip has GPU, you don't need to add these two lines. So you need generate two SDKs, one support GPU,  one for chips like i.MX6ULL without GPU. And i don't shutdown GPU, these two lines just remove opengl flags when configure qt3d.

0 Kudos
Reply
1,129 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @2458332461 

I am testing.

0 Kudos
Reply
1,297 Views
Maruti
Contributor II
Hii,
Im compiling sdk for iMX93 Linux 6.1.22 and also i followed the same method that i have added those two lines in conf/local.conf file of my build folder but the error still exists.
Below are the two errors
error1
======
ERROR: qtdatavis3d-6.5.0-r0 do_install: ExecutionError('/mnt/xvdb1/Maruti/PRHUZ/imx-yocto-bsp/build-imx93-sodimm/tmp/work/armv8a-poky-linux/qtdatavis3d/6.5.0-r0/temp/run.do_install.3523202', 1, None, None)
ERROR: Logfile of failure stored in: /mnt/xvdb1/Maruti/PRHUZ/imx-yocto-bsp/build-imx93-sodimm/tmp/work/armv8a-poky-linux/qtdatavis3d/6.5.0-r0/temp/log.do_install.3523202

error2
=====
ERROR: Task (/mnt/xvdb1/Maruti/PRHUZ/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qtdatavis3d_git.bb:do_install) failed with exit code '1'
ERROR: qt3d-6.5.0-r0 do_install: ExecutionError('/mnt/xvdb1/Maruti/PRHUZ/imx-yocto-bsp/build-imx93-sodimm/tmp/work/armv8a-poky-linux/qt3d/6.5.0-r0/temp/run.do_install.3523275', 1, None, None)
ERROR: Logfile of failure stored in: /mnt/xvdb1/Maruti/PRHUZ/imx-yocto-bsp/build-imx93-sodimm/tmp/work/armv8a-poky-linux/qt3d/6.5.0-r0/temp/log.do_install.3523275

Can you please suggest some better method.

Thanks,
Maruti Naik

0 Kudos
Reply