imx6ul yocto sources codes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul yocto sources codes

1,133 次查看
liangfeng_0824
Contributor I

i.MX8 yocto the newest version:     L4.9.88_2.0.0-ga         05/2018       i.MX 7ULP and i.MX 8MQuad GA   release
i.MX6ul yocto the newest version:  L4.1.15_2.0.0_ga        10/2016       Added i.MX 6ULL and updates to Yocto Project Krogoth

I use i.MX6ul platform now . Can i use L4.9.88_2.0.0-ga by setting up MACHINE=imx6ulevk ?
$ DISTRO=<distro name> MACHINE=<machine name> source fsl-setup-release.sh -b <build dir>
$ bitbake fsl-image-qt5-validation-imx

标签 (2)
0 项奖励
回复
3 回复数

787 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Liang Feng,

The L4.9.88_2.0.0 BSP Release does also support the i.MX6ULL EVK as shown on the Build Configurations section of the i.MX Yocto Project User's Guide (available as part of the BSP documentation bundle).

The MACHINE would be imx6ulevk if you are using the i.MX6UL EVK

However, the sfl-image-qt5-validation-imx image cannot be built for the i.MX6UL EVK as Qt5 requires a GPU for Graphic Hardware Acceleration.

I hope this information helps!

Regards,

0 项奖励
回复

787 次查看
liangfeng_0824
Contributor I

Why is there no one replying?

0 项奖励
回复

787 次查看
liangfeng_0824
Contributor I

怎么没有人回复?

0 项奖励
回复