Hello,
I've sent You some comments directly.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
Hello,
really glad to receive your response.
I am now grounding JTAG_MOD. Boot_mode0 is selected as 1 boot_mode1 is selected as 0, and the PC is connected via USB_OTG1, but the boot utility is always such an interface.
There is also a phenomenon. Although I have not started the board after power-on, the current is always 5V-120ma. Is this normal?
===
Hello,
Looks like the i.MX6SX does not start at all.
Use recommendations of Chapter 4 (Avoiding Board Bring-up Problems)
in the i.MX6SX Hardware Development Guide.
https://www.nxp.com/files-static/32bit/doc/user_guide/IMX6SXHDG.pdf
Regards,
Yuri.
Have a question to confirm with you, the LICELL pin of the PMIC chip I am currently floating, so there will be problems? Must I pick up a button battery in this place?
Hello,
A capacitor to ground on the LICELL must be present.
Regards,
Yuri.
Hello,
use additonally console log. It helps to clarify the issue.
Regards,
Yuri.
Hello, I am still not booting properly here. I will use the MfgTool2 software to download the firmware via USB_OTG to the interface ""loading U-boot". What is this because of this?