imx6solox无法启动

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6solox无法启动

11,165 Views
kai1
Contributor I

大家好,我公司在用MCIMX6X4EVM10AB 做一个项目。现在遇到了板子不启动的问题,现象如下:

供电都正常,但是无论配置到qspi1  启动还是 SD2 启动,用示波器都测量CLK都没有信号输出,实在找不到原因,下面是我的原理图,请大神帮忙指点一下。

Labels (1)
0 Kudos
13 Replies

10,816 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  I've sent You some comments directly.

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos

10,816 Views
kai1
Contributor I

您好,

很高兴收到您的回复。

我现在把JTAG_MOD ,接地了。boot_mode0选为1 boot_mode1选为0,通过USB_OTG1连接PC,但是boot utility始终是这样的界面。

还有一个现象,我这边上电后,板子虽然没有启动,但是电流始终是 5V-120ma,这样的现象是否正常呢?

0 Kudos

10,816 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  really glad to receive your response.

 

  I am now grounding JTAG_MOD. Boot_mode0 is selected as 1 boot_mode1 is selected as 0, and the PC is connected via USB_OTG1, but the boot utility is always such an interface.

 

  There is also a phenomenon. Although I have not started the board after power-on, the current is always 5V-120ma. Is this normal?

===

Hello,

   Looks like the i.MX6SX does not start at all.

Use recommendations of Chapter 4 (Avoiding Board Bring-up Problems)

in the i.MX6SX Hardware Development Guide.

https://www.nxp.com/files-static/32bit/doc/user_guide/IMX6SXHDG.pdf 

Regards,

Yuri.

0 Kudos

10,816 Views
kai1
Contributor I

hi,

有个问题想和您确认一下,PMIC芯片的LICELL引脚我目前是悬空状态,这样会有问题吗?这个地方一定要接一个纽扣电池吗?

0 Kudos

10,816 Views
Yuri
NXP Employee
NXP Employee

Have a question to confirm with you, the LICELL pin of the PMIC chip I am currently floating, so there will be problems? Must I pick up a button battery in this place?

Hello,

  A capacitor to ground on the LICELL must be present. 

Regards,

Yuri.

0 Kudos

10,816 Views
kai1
Contributor I

hi,

Another apearance is that USB_OTG1 can be recongnized by PC,when POR is connected with test pen ofoscilloscope.

what is your idea about the problem?

0 Kudos

10,816 Views
Yuri
NXP Employee
NXP Employee

Is there POR assertion circuit  (supervisor)?

0 Kudos

10,816 Views
kai1
Contributor I

您好,

我这边现在还是启动不正常,通过USB_OTG用MfgTool2 软件下载固件会卡到这个界面“”“loading U-boot ”,请问这是因为什么呢?

0 Kudos

10,816 Views
Yuri
NXP Employee
NXP Employee

Hello,

  use additonally console log. It helps to clarify the issue. 

Regards,

Yuri.

Hello,     I am still not booting properly here. I will use the MfgTool2 software to download the firmware via USB_OTG to the interface ""loading U-boot". What is this because of this?

https://community.nxp.com/servlet/JiveServlet/download/1219438-1-457830/3403F808%401F18ED04.86C9A65D

0 Kudos

10,816 Views
kai1
Contributor I

My schematic diagram is in enclosure , maybe there is something wrong with it.

0 Kudos

10,816 Views
kai1
Contributor I

The POR pin of imx6 is connected with RESET_MCU pin of PMIC.

0 Kudos

10,816 Views
kai1
Contributor I

hi dear,

Thank you very much for your help !

USB_OTG1 has been recognized by PC ,here is the screenshot of boot utility, then how can i find the problem about startup

0 Kudos

10,816 Views
Yuri
NXP Employee
NXP Employee

Hi,

  According to the screenshot the i.MX6SX starts in serial downloader mode. 

Try using other boot mode / devices.

Regards,

Yuri.

0 Kudos