imx6q uboot logo problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q uboot logo problem

Jump to solution
1,424 Views
yuhundehao
Contributor III

I've patched the patch logo。

bsp:uboot2009 linux-3.0.35.

Such as the picture should be displayed in the red box on the left side of the show, now displayed on the right side of the display, which is what causes

pastedImage_3.jpg

Labels (1)
0 Kudos
Reply
1 Solution
1,184 Views
yuhundehao
Contributor III

The problem has been solved for the following reasons:

<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=1 seek=6291456 skip=70">Write Log</CMD>

Skip patch requirements are 54, first changed to 70, up to the big demand。

View solution in original post

0 Kudos
Reply
4 Replies
1,185 Views
yuhundehao
Contributor III

The problem has been solved for the following reasons:

<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=1 seek=6291456 skip=70">Write Log</CMD>

Skip patch requirements are 54, first changed to 70, up to the big demand。

0 Kudos
Reply
1,184 Views
yuhundehao
Contributor III

Do I have a problem with this  0001-Enable-uboot-logo-for-HDMI-LCD-and-LVDS.patch?

0 Kudos
Reply
1,184 Views
igorpadykov
NXP Employee
NXP Employee

had you adjusted timings for custom lcd:

How to change SABRE-SD screen resolution in LOLLIPOP(5.0.0? 

0 Kudos
Reply
1,184 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuhundehao

please try uboot logo patches from

https://community.freescale.com/docs/DOC-98109 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply