hi nxp,
the mfgtools of Android 7.1.2_2.0.0 for imx6q not work;
I download the android_N7.1.2_2.0.0_tools.tar.gz form nxp.com, and unzip it, but there is no mfgtools.tar.gz, but have mfgtools.zip, the size is only 4.28Mbytes; after unzip, the sub dir is clean;
thanks for help !
解決済! 解決策の投稿を見る。
Hi,
So sorry for late reply. Due to our network problem, I can not login in and give reply to you. Here the newest android_N7.1.2_2.0.0_tools.tar.gz mfgtool in our website has been realeased now, you can donwnload it. It works well. Thanks a lot for your quesions.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
6 days, nobody know the this problem, just tools problem
It's the tool problem, and the it has update in our website, please have a check.
update:
partition-table.img is the new img file on andorid 7.1.2 release; but the ucl2.xml from the previous mfgtool release not have partition-table.img, so the partition-table.img not flashing to the board;
the borad can not bring up after flashing with the previous mfgtool, can't find partition:boot;
this is the log:
U-Boot 2017.03 (Sep 20 2017 - 00:38:39 +0800)
CPU: Freescale i.MX6Q rev1.5 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 38C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
flash target is MMC:2
Net: No ethernet found.
can't find partition: misc, dump the partition table
idx 0, ptn 0 name='gpt' start=0 len=2048
idx 1, ptn 0 name='bootloader' start=2 len=2046
idx 2, ptn 1 name='mmcsdc1' start=16384 len=65536
idx 3, ptn 2 name='mmcsdc2' start=83968 len=65536
idx 4, ptn 0 name='' start=0 len=0
cannot get the partion info for misc
Cannot find partition 4080
do_raw_read failed, ret 1
read_bootctl, bcb_rw_block read failed
read command failed
Hi,
So sorry for late reply. Due to our network problem, I can not login in and give reply to you. Here the newest android_N7.1.2_2.0.0_tools.tar.gz mfgtool in our website has been realeased now, you can donwnload it. It works well. Thanks a lot for your quesions.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
If the directory does not exist, create the android/sabresd directory under MFGTool-Dir/Profiles/Linux/OS Firmware/
files/.
You can rerfer to the "Android_Quick_Start_Guide.pdf" as our engineer told you above.
Hi Rita Wang,
can you opened the tool on android7.1.2? i still opened failed !
Hi,
I will try to download the demo images and ues the mfgtool to dowload the images to my i.MX6Q board. And then give you reply.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
N7.1.2. MFG tool package on the Web is empty. Please look at "Android_Quick_Start_Guide.pdf",
in particular at section 3.3 (Flashing board images) how to use files from OS (demo) images, that may be
found on the Web.
https://community.nxp.com/docs/DOC-335604
Regards,
Yuri.
yes,i try to flash the demo images, but the MFG tool can not open, does some files in the N7.1.2. MFG tool package missing?
Hi,
I have try download and unzip it. The mfgtools.zip is 4.28Mbytes and you need to unzip it. Then you can see all the mfgtool files here
Here you can try to download the tool again, the link is :
https://www.nxp.com/webapp/sps/download/preDownload.jsp
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
first thanks for your response; and i means after unzip the mfgtools.zip, all sub dir is empty, mfgtools can not opened;
the size of mfgtools.zip on andorid 7.1.1 version is 62.4Mbytes, all sub dir have files; Document, Drivers, Profiles etc. and it work fine on android 7.1.1; but android7.1.2 can not open;