Hi everyone,
I'm new in a community, on a forum and into imx6 linux development.Though i had experience with linux embedded on a ATNGW100.
Currently i;m working on a board with imx6q.
I have to run a lvds screen. It's connected with a imx6 through 2 channels 4 pairs each.
Unfortunately i can't run it.
Frankly, i don't know where the problem is.
Or is it a device tree configuration, or uboot command line settings.
I'm using community yocto bsp based on a sabresd machine.
What i did is disable a hdmi.
LVDS panel is a M240HTN01.2.
I've attached dmesg, bootargs and a device tree config files.
I wonder if someone could direct me where to find a knowledge to pass this issue?
Thanks!
Original Attachment has been moved to: files.bz2
已解决! 转到解答。
HI Sebastian
first, one needs to add timings for that LCD, please check some examples
for struct fb_videomode
how to support WSVGA output in imx6sdq
http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/
for lvds split mode settings one can check attached patch and link below
Re: i.MX6Q LVDS split mode outputs LVDS1 only
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Sebastian
first, one needs to add timings for that LCD, please check some examples
for struct fb_videomode
how to support WSVGA output in imx6sdq
http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/
for lvds split mode settings one can check attached patch and link below
Re: i.MX6Q LVDS split mode outputs LVDS1 only
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sebastian,
what do you mean when you say that you can't run it? I mean, is there any signal coming out or it does nothing at all? Maybe the problem is the same reported here
Just modifying clk-imx6q.c does the trick
Hope it helps
Hi Igor,
I am a beginner for iMX6 and android. Currently, I am working with iMX6 quad sabre sd board with android OS.
I want to implement/debug applications related to image/video/audio processing/LCD interface on iMX6.
Can you please suggest me what software/IDE I can use for coding.
Regards,
Bharathi