MCU : imx6
Kernel : L3.0.35_4.1.0
- When I use memcopy from ddr to eim(using ioremap), memcopy function is good.
- So, I think there is no problem with eim settings.
SDMA test sample : unitest - mxc_sdma_memcopy_test.c sample source
- mem to mem test is good using sample source. (from DDR to DDR)
SDMA firmware version is .1(imx6q)
My plan is data transmission from DDR to EIM(FPGA) using SDMA.
I changed the address of wbuf or rbuf to EIM address(using ioremap_nocache to change to virtual memory), but chip select not responding.
Simply, I just modified the memory address(rbuf->eim virtual address or wbuf->eim virtual address) in the sample source.
But did not succeed
Hi jieh
one can look at example mxc_sdma_memcopy_test.c in imx-test-3.0.35 package
Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
thank you for your reply
I am now reference mxc_sdma_memcopy_test.c
DDR replication to DDR has succeeded, but when I changed my target address to an EIM virtual address (iimmap physical address via ioremap_nocache into a virtual address), the test DMA failed
Hi jieh,
I have the same question with you.
board: i.MX6Q, Android version:4.4.2, Kernel version:3.0.35.
I need transfer data from EIM to mx6q internal memory.
I have mapped EIM address like below:
s_armaddr = ioremap_nocache(WEIM_ARB_BASE_ADDR, SDMA_BUF_SIZE );
And then i set the source buf like below:
sg_set_buf(&sg[0], s_armaddr + 0x16, SDMA_BUF_SIZE );
But the data i read form eim is not what i want.
Have you resolved the question? And could you give me some suggestions please?
Thank you.
Best Regards