Hello,
we have to support am 1280x800 display with single lvds channel. A display clock with 68 MHz is required. We're using the 3.10.17 kernel.
Everthing is ok when i set the pixel clock to 42.5 MHz and below. Higher clocks do not work but should since the imx6dl should deliver 85 MHz.
Thank you for helping.
Best regards,
Ludwig
解決済! 解決策の投稿を見る。
Hi Ludwig
LDB clock can provide up to 85 MHz.
Please check your clock tree. Set correct parent clock according to your requirement.
After debugging the clock initialization i tried different hardware. It was a hardware defect.
Thank you for your support.
Best regards,
Ludwig
Hi Ludwig
LDB clock can provide up to 85 MHz.
Please check your clock tree. Set correct parent clock according to your requirement.
Thank you for your response.
Can you tell me where it should be done in the kernel code?
I was able to change ldb_di1_clk_sel but was not able to adjust ldb_di1_ipu_div.
if splashscreen is enabled in uboot (CONFIG_SPLASH_SCREEN )
one can check ..board/mx6qsabresd/mx6qsabresd.c setup_display(void)
Best regards
igor