imx6dl-Android lollipop Ethernet issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6dl-Android lollipop Ethernet issue

822件の閲覧回数
小樺陳
Contributor I

my os: android 5.0

platform:imx6dl

It happened when i download default source code

When i ping to www.google.com

it will fail

my setting as below

ping 210.242.127.54 ==>0K (host:www.google.com)

ping www.google.com==>fail

#getprop | grep

dhcp.eth1.dns1:10.1.0.19

dhcp.eth1.dns2:10.1.0.17

0 件の賞賛
返信
1 返信

655件の閲覧回数
b36401
NXP Employee
NXP Employee

Possibly the board has no route to the network your DNS servers 10.1.0.17 and 10.1.0.19 are located in.

So the system fails to resolve www.google.com name into 210.242.127.54 IP.

Please try to set 8.8.8.8 DNS server instead.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信