Hi,
I'm having an issue setting the resolution of a LVDS display to 1280*800 - Wide Screen. The kernel on our custom board is fsl-release-bsp and Jethro version 3.14.52 (duallite).
My research shows that this version should use panel=LDB-WXGA and not the boot-args but neither way actually works. Halting uboot shows "unsupported panel LDB-WXGA" question is how and what can I do to get my screen found at the corrent resoultion? The default Hannstar is fine but the last 1/4 is scrambed on this screen.
Also does the device tree have to find this display via an i2c probe or can I simply adjust the resoultion to 1280*800 somewhere using the defult Hannstar driver? Can somebody explain this boot procedure for the 3.14.52 kernel?
Thanks,
Edward
解決済! 解決策の投稿を見る。
Hi Edward,
Yes you need to modify the device tree in order to change the display setup, bootargs are not used any more.
Here is where the Hannstar display is specified for the SabreSD, the node contains both the resolution and the timings of the display:
linux-2.6-imx.git - Freescale i.MX Linux Tree
Hope this helps.
Regards,
Gary
Please refer to the following community threads:
https://community.freescale.com/docs/DOC-172312
https://community.freescale.com/message/590530
Hope this will be helpful.
Best Regards,
Artur
Hi Edward,
Yes you need to modify the device tree in order to change the display setup, bootargs are not used any more.
Here is where the Hannstar display is specified for the SabreSD, the node contains both the resolution and the timings of the display:
linux-2.6-imx.git - Freescale i.MX Linux Tree
Hope this helps.
Regards,
Gary
Hi Gary,
100% spot on! Worked. By the way I noticed in another link a structure defined as:
timing3: LDB-WXGA {
clock-frequency = < ........
Would this be the definition of LDB-WXGA used in a only remaining display boot-arg "panel=LDB-WXGA" tweak?
Thanks again,
Edward.