imx6 mass production memory calibration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 mass production memory calibration

Jump to solution
936 Views
yairh
Contributor III

Hi, 

After reviewing  the information in

https://freescale.jiveon.com/docs/DOC-105652

https://freescale.jiveon.com/docs/DOC-346065 

We still would like to know how to run memory calibration for mass production purposes. 

It seems the the the UI version cannot be executed in "batch mode" generating calibration parameters after each cycle. The two other option described in https://freescale.jiveon.com/docs/DOC-105652 are used fro memory stress test and not generation of calibration parameters. 

Is there a way to generate calibration parameters in a non-interactive mode? We would like to run the calibration on a large sample of our product. 

 

Thanks,

Yair 

0 Kudos
Reply
1 Solution
918 Views
yairh
Contributor III

@Yuri 

Thanks for the information. Will review the application note. 

 

Yar

View solution in original post

0 Kudos
Reply
2 Replies
923 Views
Yuri
NXP Employee
NXP Employee

@yairh 
Hello,

   Generally section 7.3 (Timing Calibrations Usage) of AN4467 (i.MX 6 Series DDR Calibration)
describes possible calibration policies.

https://www.nxp.com/docs/en/application-note/AN4467.pdf

  Usually it is enough to calibrate manually several boards from a batch under different
operation conditions and use average / median values for all boards.

  We do not have special calibration tool as You need.

Regards,
Yuri.

0 Kudos
Reply
919 Views
yairh
Contributor III

@Yuri 

Thanks for the information. Will review the application note. 

 

Yar

0 Kudos
Reply