lvds display error color,backgorund color should be black,i have checked related parameter ,but not solved,and hdmi display well
lcd:24bit,RGB24
Hi sunyd
one can check simila issue
also one can try changing the DI clock polarity, bit to change
IPUx_DI0_GENERAL bit17
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
and if=RGB666/888 ldb=dul0,display this condition;
but, if change the ldb from dul0 to sin0,display black screen(display null)
on linux( kernel3.0 .035),display well,
just below
thanks
hi,igorpadykov,
modified ("#define DI_GEN_POLARITY_DISP_CLK (1 << 17)") 1 to 0("0<< 17"),but the bad color show the same previous,
and what else to do?
thanks for yours
suggest to use 1360 resolution, as strictly speaking 1366 resolution
doesn't work with the IPU and GPU because that resolution is not multiple of 8.
Best regards
igor
hi,igo:
the error color is still crazy, have you any other suggestions?
i'm sorry to give you trouble,
thanks
formally this is no supported by hardware, so there are no formal suggestions.
You can just try experimenting by own luck.
Best regards
igor