lvds display error color,backgorund color should be black,i have checked related parameter ,but not solved,and hdmi display well
lcd:24bit,RGB24
Hi sunyd
one can check simila issue
also one can try changing the DI clock polarity, bit to change
IPUx_DI0_GENERAL bit17
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
suggest to use 1360 resolution, as strictly speaking 1366 resolution
doesn't work with the IPU and GPU because that resolution is not multiple of 8.
Best regards
igor
formally this is no supported by hardware, so there are no formal suggestions.
You can just try experimenting by own luck.
Best regards
igor