hello everyone,i have a problem in i2c1 in imx53.
when i operation i2c bus , i2sr_ibb alway is detect ibb=1; i do not why ?
i don't know this is a software problem or hardware problem ? i need help.
root@freescale ~$ hwclock -w
rtc-pcf8563 1-0051: pcf8563_set_datetime: secs=13, mins=11, hours=11, mday=1, mon=0, year=70, wday=4
i2c i2c-1: master_xfer[0] W, addr=0x51, len=2
i2c i2c-1: <i2c_imx_xfer>
i2c i2c-1: <i2c_imx_start>
i2c i2c-1: <i2c_imx_bus_busy>
i2c i2c-1: <i2c_imx_bus_busy> I2C bus is busy
i2c i2c-1: <i2c_imx_stop>
i2c i2c-1: <i2c_imx_bus_busy>
i2c i2c-1: <i2c_imx_xfer> exit with: error: -110
rtc-pcf8563 1-0051: pcf8563_set_datetime: err=-110 addr=02, data=13
hwclock: RTC_SET_TIME: Input/output error
i2c devices addr is right,and i use eim_d16 and eim_eb2 as i2c-1 pin
MX53_PAD_EIM_D16__I2C2_SDA,
#define MX53_PAD_EIM_D16__I2C2_SDA (_MX53_PAD_EIM_D16__I2C2_SDA | MUX_PAD_CTRL(MX53_I2C_PAD_CTRL_1))
#define _MX53_PAD_EIM_D16__I2C2_SDA IOMUX_PAD(0x460, 0x118, 5, 0x820, 1, 0)
MX53_PAD_EIM_EB2__I2C2_SCL,
#define MX53_PAD_EIM_EB2__I2C2_SCL (_MX53_PAD_EIM_EB2__I2C2_SCL | MUX_PAD_CTRL(MX53_I2C_PAD_CTRL_1))
#define _MX53_PAD_EIM_EB2__I2C2_SCL IOMUX_PAD(0x45C, 0x114, 5 | IOMUX_CONFIG_SION, 0x81C, 1, 0)
解決済! 解決策の投稿を見る。
Hello,Zidong,
It seems that you connected a RTC IC on I2C2 bus, Please measure 32.768k crystal for RTC by oscilloscope, I feel this crystal doesn't work !
if the waveform is OK, we can check others .
Regards,
Weidong
Hi all,
I have a problem with I2C on imx6Solo.
Here is my environment: Processor: imx6Solo, OS: Windows embedded compact 2013. Board: Custom.
imx6solo is connected with a touch controller via I2C. When the device boots, everything seems ok but after first touch on the screen (which means after first I2C read or write operation) I2C hangs.(apparently, device hangs).
My observations are:
1. ) Interrupt coming from screen touch can be detected. I can see this fact on the console output. (Every touch IRQ is logged to serial trace)
2. )After single touch on the screen, read and write requests are seen periodically.
3.) The I2C protocol flow is here:
Grant Bus Master -> change to receive mode -> Ensure the Start operation is DONE.
To ensure the start operation is done, check if IBB bit is set to 1(which means I2C is busy). The problem arised here. IBB bit is never set to 1!! in other words stucks at ZERO. I am checking this case several times and after a while gives such an error "I2C Generate Start can't launch".
4.) Second finding is SDA line. I probed the I2C lines and observed that when the device wake up, both I2C line states seem ok.(both stay high) but after first touch SDA stucks at ZERO!!! When the line is observed for a while, sometimes it gets high for a short time but then goes back to low which does not make sense.
I believe that the problem should not be too hard and i am missing a point. Could you all please help me for this issue? What can the reason of this problem be?
Thanks in advanced,
Best regards
Hello,Zidong,
It seems that you connected a RTC IC on I2C2 bus, Please measure 32.768k crystal for RTC by oscilloscope, I feel this crystal doesn't work !
if the waveform is OK, we can check others .
Regards,
Weidong
Hello,Pan
Did you resolve your quesions ?
Weidong
Hello, Pan,
How about your RTC ?
weidong
thank you,sir i had solve the problem.