Hi
when i insert USB with wifi dongle i see imx28 is getting shut down
following are the log
Following is the log
[ 102.640000] mxs-battery mxs-battery.0: vdd5v droop interrupt occurred
[ 102.640000].Done, shutting down
[ 102.640000] Successfully sent signal
[ 102.640000] mxs-battery mxs-battery.0: new 5v disconnection detected
[ 102.660000] ehci_fsl_bus_resume, Host 1
Hi shashikant
USB wifi dongles may require much current and i.MX28 can be turned off
due to brown out events, as described in Chapter 11 Power Supply Reference Manual,
one can try to debug it. May be useful to look at
https://community.nxp.com/docs/DOC-95515
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks igor,
for the link
so what we have options to try , if you elaborate would be helpful.
i have
1. brownout irq to be disable to try,
2.
/* Enable the following if you only have a DCDC_BATT source only and no V
* This includes configurations with and without a supercap on the BATTERY pin as
* shown in the i.MX28 reference schematic (applies to i.MX233 as well).
*
* NOTE: If both a DCDC_BATT and VDD5V source are present, this is not meant to
* select which one to use. This is only for hardware configurations this no
* VDD5V power source.
*/
#define NO_VDD5V_SOURCE
but dont know whats the consequence of it
any other best fix would be appreciated
one can try to debug it, using for example AN4553
Using Open Source Debugging Tools for Linux on i.MX Processors
Best regards
igor
On further debug on with battery,
usb - wifi not connected, i am getting following log
[ 86.940000] mxs-battery mxs-battery.0: new 5v disconnection detected
[ 86.940000] mxs-battery mxs-battery.0: vdd5v droop interrupt occurred
[ 86.940000] mxs-battery mxs-battery.0: vdd5v droop interrupt occurred
[ 86.940000] mxs-battery mxs-battery.0:ddi_power_handle_vdd5v_droop 8b00
[ 86.940000] mxs-battery mxs-battery.0:.Done, shutting down
[ 86.940000] mxs-battery mxs-battery.0: Successfully sent signal
[ 86.990000] mxs-auart mxs-auart.3: Unhandled status 52068d 220b01
[ 86.990000] mxs-auart mxs-auart.3: Cleared TX Data Count & Pulled RTS low,
[ 86.990000] UART Status --> 5206dd
[ 86.990000] , UART Control reg -> 220b01
[ 86.990000] mxs-auart mxs-auart.4: Unhandled status 52028d 220b01
[ 87.110000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 87.210000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 87.310000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 87.410000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 87.510000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 87.610000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 87.710000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 87.810000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 87.910000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 88.010000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 88.110000] mxs-battery mxs-battery.0: state machine failed to schedule
[ 88.210000] mxs-battery mxs-battery.0: state machine failed to schedule
why this we are getting
state machine failed to schedule??
from log: [ 86.940000] mxs-battery mxs-battery.0: vdd5v droop interrupt occurred
obviously this is power supplies issue, usb dongle consumes too much power from board.