Hi,
When I use IPU to resize image. Sometimes, it was failed and kernel panic. (The image resolution is : 1280 x 720)
I get the flowing error:
" imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000 "
Thanks.
Yonghe.Luo
已解决! 转到解答。
Hi Yonghe.Luo
IPU_INT_STAT_10 = 0x40000000 means AXI read access error, one can check
programming requirements provided for AXIR units in sect.37.4.2.4.1 Handling real time channels,
37.4.2.5, Table 37-15 i.MX6DQ Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yonghe.Luo
IPU_INT_STAT_10 = 0x40000000 means AXI read access error, one can check
programming requirements provided for AXIR units in sect.37.4.2.4.1 Handling real time channels,
37.4.2.5, Table 37-15 i.MX6DQ Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------