imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000

ソリューションへジャンプ
1,376件の閲覧回数
yongheluo_hotma
Contributor III

Hi,

    When I use IPU to resize image. Sometimes, it was failed and kernel panic. (The image resolution is : 1280 x 720)

    I get the flowing error:

    " imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000 "

   Thanks.

    Yonghe.Luo

0 件の賞賛
返信
1 解決策
1,062件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yonghe.Luo

IPU_INT_STAT_10 = 0x40000000 means AXI read access error, one can check

programming requirements provided for AXIR units in sect.37.4.2.4.1 Handling real time channels,

37.4.2.5, Table 37-15 i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,063件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yonghe.Luo

IPU_INT_STAT_10 = 0x40000000 means AXI read access error, one can check

programming requirements provided for AXIR units in sect.37.4.2.4.1 Handling real time channels,

37.4.2.5, Table 37-15 i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,062件の閲覧回数
yongheluo_hotma
Contributor III

Dear Igor,

     Thanks.

    

    Yonghe.Luo

0 件の賞賛
返信