imx RT 1176 Serial download mode lpuart channel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx RT 1176 Serial download mode lpuart channel

Jump to solution
545 Views
Kris_chao
Contributor III

I have a question. For imx RT 1176 chip, when change the boot mode to enter in serial download mode, does the host communicate with the BootRom must be in LPUART1? or we can select the LPUART channel by myself?

0 Kudos
1 Solution
529 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) does the host communicate with the BootRom must be in LPUART1? or we can select the LPUART channel by myself?
-- Yes, it must use the LPUART1.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
530 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) does the host communicate with the BootRom must be in LPUART1? or we can select the LPUART channel by myself?
-- Yes, it must use the LPUART1.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos