--------------------------------------------------------------------------------------------------
SETTING:
PLL_ARM divider set to 16, Clock divider set to 0.
Thus, ARM clock root = 24 / 2 * 16 / ( 0 + 1)
= 192 Mhz
--------------------------------------------------------------------------------------------------
CODE:
while(1){
counter++;
if (counter >= 0x40000000){ // if counter >= 1 Giga
toggleGPIOPIN();
resetCounter();
}
}
--------------------------------------------------------------------------------------------------
FOR 'counter++' part, 3 line assembly code is generated by the compiler:
LOAD
ADD
BRANCH
--------------------------------------------------------------------------------------------------
Thus at least 3 clock cycle for the 'counter++' loop.
Time between GPIO PIN toggle should be at least = (3 x 1 Gig) / 192 Meg
= 15.625 second
BUT the problem occur. Time between GPIO toggle is ~5 second (measure by oscilloscope)
Means the arm clock root running at least = 5 / (3 x 1Gig)
= 600 Mhz
--------------------------------------------------------------------------------------------------
I did try to set arm clock root to 800Mhz, but the result shows it run more then 2GHz.
WHAT IS HAPPENING??
Hi Anson,
if you are speaking about CCM_ANALOG_PLL_ARMn
DIV_SELECT can not be 16. Valid range for divider value: 54-108.
Fout = Fin * div_select/2.0.
Sect.18.5.1.3.1 "ARM PLL" i.MX6DQ RM states:
"This PLL synthesizes a low jitter clock from a 24 MHz reference clock. The clock output
frequency for this PLL ranges from 650 MHz to 1.3 GHz. The output frequency is
selected by a 7-bit register field CCM_ANALOG_PLL_ARM[DIV_SELECT].
PLL output frequency = Fref * DIV_SEL/2"
Also it may be useful to check arm clock root
with CCM_CCOSR.
Best regards
chip
I tried your suggestion, clkout result is not correct as well.
--------------------------------------------------------------------------------------------------------------------------------------------------------------
ARM Clock Setting:
PLL_DIV => 54
CLK_DIV => 7
PLL_ARM = 24 * PLL_DIV / 2
= 24 * 54 / 2
= 648 MHz
ARM CLOCK ROOT = PLL_ARM / (CLK_DIV + 1)
= 648 / (7 + 1)
= 81 MHz
---------------------------------------------------------------------------------------------------------------------------------------------------------------
CCM_CCOSR Setting:
CCOSR_DIV => 8
---------------------------------------------------------------------------------------------------------------------------------------------------------------
aspected clkout = ARM CLOCK ROOT / CCOSR_DIV
= 81 / 8
= 10.125 MHz
But result measure is = 5.051 MHz
Hi Anson,
what software and board are you using ?
I would suggest to printf all registers for example
(CCM_CACRR) and its "arm_podf' value and others.
All clock generation paths one can find in Chapter 18
i.MX6DQ RM. Even better to use SDK
i.MX 6Series Platform SDK : Bare-metal SDK
Best regards
chip
Board: Boundary Nitrogen6x with imx6q
Hi Anson,
I would suggest to check with SDK
i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series
Best regards
chip
CCM_ANALOG_PLL_ARM (Addr: 0x20C_8000) Value: 0x80002036
CCM_CACRR (Addr: 0x20C_4010) Value: 0x7
CCM_CCOSR (Addr: 0x20C_4060) Value: 0x01EA0001
IOMUXC_SW_MUX_CTL_PAD_GPIO03 (Addr: 0x20E_022C) Value: 0x4
Output Measure at: clko2
OS: QNX