imx6q: u-boot: dual channel LVDS (split mode)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q: u-boot: dual channel LVDS (split mode)

2,624件の閲覧回数
pj0585
Contributor III

Hi,

I have a custom hardware based on imx6qsabresd. I'm using dual channel LVDS display (1680x1050), LVDS split mode.

I need to enable UBoot splash image. Any one attempted to enable LVDS split mode in Uboot ?

I'm using ltib's u-boot (2009.08)

Any inputs will be on help?

- Pj

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,431件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Are you using Ubuntu or Android?

Best Regards,

Alejandro

0 件の賞賛
返信

1,431件の閲覧回数
liyu1
Contributor III

I have such a demand !

                  Thanks! 

0 件の賞賛
返信

1,431件の閲覧回数
pj0585
Contributor III

Hi Alejandro,

Would it make a difference in U-Boot whether I use Ubuntu or Android?

I'm not using either. I'm using Yocto's linux BSP.

-Pj

0 件の賞賛
返信