iMX8mq emmc flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8mq emmc flashing

842 次查看
abhilashyarrago
Contributor I

Hi,

We are working on iMX8MQ based custom board and facing issue while flashing image into eMMC using UUU utility on Linux 16.04.

We tried flashing with SD card, Facing issue while booting on one iMX8mq platform.

The same image is working fine on another iMX8mq platform.

Please provide steps to flash Linux image to emmc on iMX8mq platform.

Thanks in Advance

标记 (3)
0 项奖励
1 回复

702 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abhilash

for custom board first it is necessary to run ddr test

i.MX8 MSCALE SERIES DDR Tool Release (V3.10) 

Then rebuild image using Chapter 4 How to bring up a new MX8MSCALE board MSCALE_DDR_Tool_User_Guide.pdf included in package, after that follow
Linux Guide from Linux 4.19.35_1.1.0 Documentation for emmc programming.

Also may be useful https://community.nxp.com/docs/DOC-343518 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励