iMX8QM MEK (imx-automotive-11) WiFi is not working with 1 YM M2 module.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM MEK (imx-automotive-11) WiFi is not working with 1 YM M2 module.

ソリューションへジャンプ
1,505件の閲覧回数
Jose1985
Contributor IV

Dear Team,

I connected a Murata 1YM M2 module for enabling Wifi and Bluetooth in iMX8QM MEK board.

https://www.embeddedartists.com/products/1ym-m-2-module/

However, when I am rebooting it seems that the WiFi module is not coming up.

The error log is as below.

 614 [   28.991573] wlan: Loading MWLAN driver                                                          
 615 [   28.996851] wlan_pcie 0000:01:00.0: enabling device (0000 -> 0002)                              
 616 [   29.003332] Attach moal handle ops, card interface type: 0x204                                  
 617 [   29.010252] PCIE8997: init module param from usr cfg                                            
 618 [   29.016448] card_type: PCIE8997, config block: 0                                                
 619 [   29.021835] cfg80211_wext=0xf                                                                    
 620 [   29.024970] sta_name=wlan                                                                        
 621 [   29.027850] uap_name=wlan                                                                        
 622 [   29.030594] wfd_name=p2p                                                                        
 623 [   29.033289] max_vir_bss=1                                                                        
 624 [   29.036044] cal_data_cfg=none                                                                    
 625 [   29.039147] ps_mode = 2                                                                          
 626 [   29.041648] auto_ds = 2                                                                          
 627 [   29.044155] fw_name=pcieuart8997_combo_v4.bin                                                    
 628 [   29.048591] rx_work=1 cpu_num=6                                                                  
 629 [   29.051910] Attach mlan adapter operations.card_type is 0x204.                                  
 630 [   29.062514] Request firmware: pcieuart8997_combo_v4.bin  
[   30.054308] wlan_dnld_fw fail ret=0xffffffff
[   30.421133] wlan_pcie: probe of 0000:01:00.0 failed with error -14
[   30.427665] wlan: Driver loaded successfully
 
Could you help me solve this issue? I think the pcie*.ko doesnt exists at
vendor/nxp-opensource/kernel_imx
 
Do you have a patch to make this work?
 
Best regards
Jose
タグ(1)
0 件の賞賛
返信
1 解決策
1,462件の閲覧回数
Jose1985
Contributor IV

Dear NXP Team,

 

I update the source to Android Automotive 11.0.0 2.3.0 and WiFi is working. However, there is a problem with Bluetooth. I shall report another issue

wlan: version = PCIE8997--16.92.10.p213.2-MM5X16266-GPL-(FP92)

 

Thanks and regards

Libin Jose

元の投稿で解決策を見る

4 返答(返信)
1,463件の閲覧回数
Jose1985
Contributor IV

Dear NXP Team,

 

I update the source to Android Automotive 11.0.0 2.3.0 and WiFi is working. However, there is a problem with Bluetooth. I shall report another issue

wlan: version = PCIE8997--16.92.10.p213.2-MM5X16266-GPL-(FP92)

 

Thanks and regards

Libin Jose

1,457件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Good news it work well. Wish you have a nice day and happy new year.

0 件の賞賛
返信
1,487件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version of BSP are you using?

0 件の賞賛
返信
1,475件の閲覧回数
Jose1985
Contributor IV

Hi Team,

We are using imx-automotive-11.0.0_1.1.0

Kernel version seems to be 5.4

Best regards,

Jose.

0 件の賞賛
返信