Right now we are working on iMX8 PCIe link. Without any PCIe device inserted in the iMX8Q evaluation board, we can get PCIe related message as below when boot up:
解決済! 解決策の投稿を見る。
Hi Jim
it is necessary to attach some device to board pcie connector
to see link up linux messages.
May be useful to check i.MX8MDQLQ EVK Board Hardware User's Guide
https://www.nxp.com/docs/en/user-guide/IMX8MDQLQEVKHUG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi I'm using the imx8mm and I'm getting similar messages. My goal is to get the Embedded Artist 1CX M.2 module up and running.
1. How do I begin to troubleshoot the issue?
2. Do we need an epdev_on regulator for pcie to work?
3. How does the ext_osc = <1> in the device tree relate to the message "pcie phy ppl can't be locked" dmesg
[ 1.983047] imx6q-pcie 33800000.pcie: 33800000.pcie supply epdev_on not found, using dummy regulator
[ 1.992612] OF: PCI: host bridge /pcie@0x33800000 ranges:
[ 1.998031] OF: PCI: No bus range found for /pcie@0x33800000, using [bus 00-ff]
[ 2.005529] OF: PCI: IO 0x1ff80000..0x1ff8ffff -> 0x00000000
[ 2.011461] OF: PCI: MEM 0x18000000..0x1fefffff -> 0x18000000
[ 2.017844] imx6q-pcie 33800000.pcie: Initialize PHY with EXT REfCLK!.
[ 2.024682] imx6q-pcie 33800000.pcie: PHY Initialization End!.
[ 2.051619] imx6q-pcie 33800000.pcie: pcie phy pll can't be locked.
[ 2.097900] imx6q-pcie 33800000.pcie: failed to initialize host
[ 2.103825] imx6q-pcie 33800000.pcie: unable to add pcie port.
Hi Jim
it is necessary to attach some device to board pcie connector
to see link up linux messages.
May be useful to check i.MX8MDQLQ EVK Board Hardware User's Guide
https://www.nxp.com/docs/en/user-guide/IMX8MDQLQEVKHUG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for the information. Just want to make sure it is expected and it is not a issue or bug before we doing further.
Best regards,
Jim