Hi,
I'm trying to dynamically configure my custom i.MX8M nano board to switch USB roles from host mode to gadget (or peripheral). I currently have my board configured as a USB host and I'm able to enumerate a USB FTDI serial device. All works as expected.
I would like to configure the dr_mode as "otg" and setup my board to either be a host device as I have today or dynamically switch it to be a USB mass storage peripheral (gadget).
I can't find any working examples and I'm hoping someone could help me. It seems when I configure my DTS to be dr_mode = "otg" with usb-role-switch enabled, I can't get any USB functionality to work. If I run some USB mass storage gadget example code, the best I get is an error "udc-core: couldn't find an available UDC or it's busy"
I'm confident my USB hardware is correct since I can run the uboot "ums mmc 2" command to make my board enumerate as a mass storage USB device. Also, as stated above, I can connect the USB to a FTDI serial port and configure it as a my DTS to be dr_mode = "host" and that works too.
I'm currently running a custom Linux build based on imx-5.10.72-2.2.0 (Yocto hardknott).
已解决! 转到解答。
I solved this today through a whole lot of trial and error.
I made my DTS for usbotg as follows:
&usbotg1 {
dr_mode = "otg";
hnp-disable;
srp-disable;
adp-disable;
disable-over-current;
usb-role-switch;
role-switch-default-mode = "host";
samsung,picophy-pre-emp-curr-control = <3>;
samsung,picophy-dc-vol-level-adjust = <7>;
status = "okay";
assigned-clocks = <&clk IMX8MN_CLK_USB_BUS>,
<&clk IMX8MN_CLK_USB_CORE_REF>;
assigned-clock-parents = <&clk IMX8MN_SYS_PLL2_500M>,
<&clk IMX8MN_SYS_PLL1_100M>;
};
And then after I configured my mass_storage device in the /sys/kernel/config/usb_gadget path, I had to do the following to get it to enumerate to my host.
echo device > /sys/bus/platform/devices/ci_hdrc.0/usb_role/ci_hdrc.0-role-switch/role
The final missing thing that I want to figure out is how to know when the host has ejected/un-mounted my mass storage USB gadget so that I can take action on what was transferred from the host to my device.
Hi @dvlogic,
No the solution you posted still doesn't work for me.
The problem I was having with udc-core was related to me adding the following config to my kernel build "CONFIG_USB_FSL_USB2" - this was a stupid cut-n-paste from some other post.
Now I am back to trying to get my device to work in gadget "peripheral" mode. The fundamental problem is my custom hardware is designed with only a USB-A port (which is doesn't expose the USB_ID pin to the external host). The USB_ID pin is floating on the hardware. In addition VBus is hardwired to +5 volts.
With the driver, I am able to set the role as "host" had communicate with external USB peripherals. However, when I set the role as gadget and program a USB gadget config, I never can get my board to enumerate to an external host.
I'm convinced there must be a software work-around since the same hardware will enumerate as a mass storage gadget device when I boot directly to U-Boot and run the command "ums mmc 2"
Let me know if you have any thoughts on where I should look for a software work-around.
Thanks!
I solved this today through a whole lot of trial and error.
I made my DTS for usbotg as follows:
&usbotg1 {
dr_mode = "otg";
hnp-disable;
srp-disable;
adp-disable;
disable-over-current;
usb-role-switch;
role-switch-default-mode = "host";
samsung,picophy-pre-emp-curr-control = <3>;
samsung,picophy-dc-vol-level-adjust = <7>;
status = "okay";
assigned-clocks = <&clk IMX8MN_CLK_USB_BUS>,
<&clk IMX8MN_CLK_USB_CORE_REF>;
assigned-clock-parents = <&clk IMX8MN_SYS_PLL2_500M>,
<&clk IMX8MN_SYS_PLL1_100M>;
};
And then after I configured my mass_storage device in the /sys/kernel/config/usb_gadget path, I had to do the following to get it to enumerate to my host.
echo device > /sys/bus/platform/devices/ci_hdrc.0/usb_role/ci_hdrc.0-role-switch/role
The final missing thing that I want to figure out is how to know when the host has ejected/un-mounted my mass storage USB gadget so that I can take action on what was transferred from the host to my device.