[iMX8M Plus] Adding machine learning libraries to Yocto reduced firmware image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[iMX8M Plus] Adding machine learning libraries to Yocto reduced firmware image

1,404件の閲覧回数
khang_letruong
Senior Contributor III

Dear Community,

I would like to know what is the necessary modification for the conf/local.conf in order to add the machine learning libraries and stuff for purpose of deploying the AI features on the board without the need of bitbaking imx-image-full, please ? Differently saying, I would like to have a firmware as minimal as possible (for example without the GUI) but it still have enough libraries (ISP, VPU, NPU) for running vision based deep learning features on board.

Thanks in advance and best regards,

Khang

0 件の賞賛
返信
1 返信

1,302件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you refer to the user guide before?

"https://www.nxp.com/docs/en/user-guide/IMX-MACHINE-LEARNING-UG.pdf"

0 件の賞賛
返信