I'm struggling with the DRAM-size in U-Boot. Our custom board solution uses a 1Gb LPDDR4 RAM, so I changed the PHYS_SDRAM_SIZE in imx8mm_evk.h to 0x4000 0000, the DDR is configured with the stress tool. But in the bootlog it still says DRAM: 2GiB.
With debug messages I traced the new set RAM size to dram_init_banksize in arch/arm/mach-imx/imx8m/soc.c.
The problem seems to be with optee, the rom_pointer[1] is set, although I removed it with
MACHINE_FEATURES_remove += "optee"
DISTRO_FEATURES_remove += "optee"
IMAGE_INSTALL_remove += "optee-test optee-os optee-client"
optee_start is at 0xbe00 000, which lies outside of my RAM-space (0x4000 000 0 - 0x8000 0000)
The banksize is defined by optee_start - PHYS_SDRAM, so because optee_start is outside of my space, the size is way to big.
Is there a way to remove optee, so the rom_pointer[1] won't be set, or otherwise to set optee_start to 0x3e00 0000? I tried to do so manually, but then the boot gets stuck at "Added memory mapping (5) : 40000000 3e000000"
已解决! 转到解答。
Hi @dpog,
You can change BL32_BASE in ATF at plat/imx/imx8m/imx8mm/platform.mk
and TEE_LOAD_ADDR at /iMX8M/ soc.mak in imx-boot to 0x7e000000 for 1GB RAM
in,OP-TEE change CFG_DDR_SIZE according to your dram size at plat-imx/conf.mk
Best Regards,
Hi @dpog,
You can change BL32_BASE in ATF at plat/imx/imx8m/imx8mm/platform.mk
and TEE_LOAD_ADDR at /iMX8M/ soc.mak in imx-boot to 0x7e000000 for 1GB RAM
in,OP-TEE change CFG_DDR_SIZE according to your dram size at plat-imx/conf.mk
Best Regards,