iMX8M Mini SOC is not powered

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8M Mini SOC is not powered

跳至解决方案
546 次查看
borisberman
Contributor III

Dear NXP Support Team,

Our client asks the following question:
What happens to the state of the IO pins of the iMX8M Mini SOC when it is not powered?
Will they be in high impedance or something else?

Thank You,
Boris

标签 (1)
0 项奖励
回复
1 解答
423 次查看
joanxie
NXP TechSupport
NXP TechSupport

got it, according to your description, these IO needs to use buffer to isolate, for what will happen, your client can refer to the data sheet as below

3.2 Power supplies requirements and restrictions
The system design must comply with power-up sequence, power-down sequence, and steady state
guidelines as described in this section to guarantee the reliable operation of the device. Any deviation
from these sequences may result in the following situations:
• Excessive current during power-up phase
• Prevention of the device from booting
• Irreversible damage to the processor (worst-case scenario)

在原帖中查看解决方案

3 回复数
519 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the IMX8MM HDG, 

joanxie_0-1712731118689.png

 

0 项奖励
回复
507 次查看
borisberman
Contributor III

Hello NXP TechSupport,

Thank you for your quick response.
I would like to clarify my question.
I didn't mean unused power rail, as described in Table#36 of IMX8MM HDG.
Our client inserts our SOM with iMX8M Mini into his device, and accordingly, SOM is powered from this device. He may have a situation where the SOM is not powered, but part of the GPIO connected to it will be powered. So the question is what will happen to the affected pins If it could cause damage to iMX8M Mini SOC, big leakage current, etc?

Best Regards,
Boris

0 项奖励
回复
424 次查看
joanxie
NXP TechSupport
NXP TechSupport

got it, according to your description, these IO needs to use buffer to isolate, for what will happen, your client can refer to the data sheet as below

3.2 Power supplies requirements and restrictions
The system design must comply with power-up sequence, power-down sequence, and steady state
guidelines as described in this section to guarantee the reliable operation of the device. Any deviation
from these sequences may result in the following situations:
• Excessive current during power-up phase
• Prevention of the device from booting
• Irreversible damage to the processor (worst-case scenario)