Hi All,
I need some direction on setting the GPR_SAI1_EXT_MCLK_EN in the IOMUXC_GPR_GPR2 register. This is to set the SAI1 MCLK as an input. I have grep'd my entire build a few times for variations of the wording for this register and there is no mention nor definition whatsoever. Normally it will be in a file such as the imx8mm-pinfunc.h or similar.
Can this register be set in the device tree or is it more 'under the hood'?
Thanks.
解決済! 解決策の投稿を見る。
Hi Edward,
You can search IOMUXC_GPR2 and I believe you can find it in the code.
In the rootfs, use the memtool to check its value, the address is 30340008.
# /unit_tests/memtool 30340008 1
E
Reading 0x1 count starting at address 0x30340008
0x30340008: 00000000
Then in the sai driver, you can try to write a value, for example:
regmap_write(the_regmap, IOMUXC_GPR2, the_value_00000001);
After updating the kernel image, use the same memtool command to check if this register modification is valid.
Good luck.
Hi Edward,
You can search IOMUXC_GPR2 and I believe you can find it in the code.
In the rootfs, use the memtool to check its value, the address is 30340008.
# /unit_tests/memtool 30340008 1
E
Reading 0x1 count starting at address 0x30340008
0x30340008: 00000000
Then in the sai driver, you can try to write a value, for example:
regmap_write(the_regmap, IOMUXC_GPR2, the_value_00000001);
After updating the kernel image, use the same memtool command to check if this register modification is valid.
Good luck.
Hi,
Thanks again that really helps! Regarding the define for IOMUXC_GPR2 I have grep'd the entire build a number of times and with variations of the wording but nothing. Do you have the define for IOMUXC_GPR2 you could email me over? Normally things like this are easily found in the pinctrl include files etc..
My build is Yocto Honister 5.15.5
Cheers.
You can refer to my search result, I'm also on 5.15
include/linux/mfd/syscon/imx7-iomuxc-gpr.h
11:#define IOMUXC_GPR2 0x08
29:#define IOMUXC_GPR20 0x50
30:#define IOMUXC_GPR21 0x54
31:#define IOMUXC_GPR22 0x58
include/linux/mfd/syscon/imx6q-iomuxc-gpr.h
13:#define IOMUXC_GPR2 0x08
sound/soc/fsl/fsl_mqs.c
316: .ctrl_off = IOMUXC_GPR2,
drivers/video/fbdev/mxc/ldb.c
160: .ctrl_reg = IOMUXC_GPR2,
170: .ctrl_reg = IOMUXC_GPR2,
222: .ctrl_reg = IOMUXC_GPR2,
282: .ctrl_reg = IOMUXC_GPR2,
drivers/gpu/drm/imx/imx-ldb.c
244: regmap_write(ldb->regmap, IOMUXC_GPR2, ldb->ldb_ctrl);
330: regmap_write(ldb->regmap, IOMUXC_GPR2, ldb->ldb_ctrl);
637: regmap_write(imx_ldb->regmap, IOMUXC_GPR2, 0);
drivers/pci/controller/dwc/pci-imx6.c
837: IOMUXC_GPR22, val,
Hi @xiaocong_fu,
Excellent! Think I need to check my word search settings... Appreciate your help and I'll let you know how I get on.
Cheers.