iMX7D MIPI and PCIe power issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX7D MIPI and PCIe power issue

跳至解决方案
727 次查看
felixhsu
Contributor III

Hi All

The customer don't use MIPI and PCIe interface, but external have link decoupling capacitor, like as below schematic.

VDDD_1P0_CAP and VDDA_PHY_1P8 and VDD_1P2_CAP measurement voltage is 0 V.  

Could you tell me VDDD_1P0_CAP and VDDA_PHY_1P8 and VDD_1P2_CAP don't pull down will have any concern?

Thanks.

schematic.jpg

标签 (3)
0 项奖励
回复
1 解答
607 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 Generally customers can use section 3.2 (Recommended connections for unused analog interfaces)
of i.MX7D Datasheet, Rev. 5, 07/2017,
where the MIPI and PCIe supply pins are recommended to be

grounded.

   It is possible to provide corresponding (correct) supply voltages for the MIPI and PCIe, when the modules

are not used.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
608 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 Generally customers can use section 3.2 (Recommended connections for unused analog interfaces)
of i.MX7D Datasheet, Rev. 5, 07/2017,
where the MIPI and PCIe supply pins are recommended to be

grounded.

   It is possible to provide corresponding (correct) supply voltages for the MIPI and PCIe, when the modules

are not used.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复