iMX6ULL + 1GB RAM DDR3L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ULL + 1GB RAM DDR3L

1,448 Views
giacomobiancala
Contributor I

Hi all,

For a new project I need to interface 1GB RAM DD3L (2 x MT41K256M16TW-107:P) to iMX6ULL.

Is it possible? The BUS width is only 16bit so I suppose it is only possible to connect a single chip MT41K256M16TW-107:P.

Thanks,

Giacomo

Labels (1)
0 Kudos
Reply
4 Replies

1,322 Views
giacomobiancala
Contributor I

Thank you Mrudang,

So can I consider that iMX6ULL is able to address 1GB RAM?

Regards,

Giacomo 

0 Kudos
Reply

1,322 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, it can work.  https://community.nxp.com/thread/508998  You can see this.

0 Kudos
Reply

1,322 Views
mrudangshelat1
Senior Contributor II

Hi Giacomo,

i.MX6ULL based EVK "SCH-29634" provided part no# for both 512MB and 1GB.

pastedImage_1.png

Regards,

Mrudang 

0 Kudos
Reply

1,322 Views
mrudangshelat1
Senior Contributor II

Hi Giacomo,

It is not possible for your suggested configuration. I suggest you use #MT41K512M16HA-125 (1 x16 bit) or equivalent.

https://www.micron.com/products/dram/ddr3-sdram/part-catalog/mt41k512m16ha-125-it 

Let me know if you have any doubts

Regards,

Mrudang

0 Kudos
Reply