My board is VAB820 (VIA), which based on imx6q , and connect adv7180 to realize parallel capture function. But when I switch the TV mode of input between PAL and NTSC , the picture will move up and down. Is there any solution to fix the problem? Thanks!!
Hi Adam
seems this is expected behaviour as with switching mode synchronization
will be lost and some time is needed to recover it.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
Could you help to explain the phenomenon of move up and down when switch TV mode between PAL and NTSC?
Thanks!
Adam
it is moving up and down due to lost synchronization.
~igor