iMX6L lack of DDR clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6L lack of DDR clock

ソリューションへジャンプ
1,068件の閲覧回数
takafuminaka
Contributor II

Hello,

We observed the lack of DDR base clock.

The clock periodically stops( 0V ).

It seems the cycle is in synchronization with LCD display's VSYNC and HSYNC.

We attached the waveform.

Could you let us know the reason about this issue?

Is this normal behavior?

Thank you.

ラベル(2)
タグ(1)
0 件の賞賛
1 解決策
938件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

This has not relation to low power modes.

During VSYNC,HSYNC i.MX6 does not fetch data

from memory, so there may be no DDR clock during LCD synch pulses.

Best regards

chip

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
938件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takafumi

if customer does not have other issues (such as OS hanging

ot other misbehaviour), then this seems as normal

behaviour. Becasue during VSYNC,HSYNC i.MX6 does not fetch data

from memory, so there may be no DDR clock during LCD synch pulses.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
938件の閲覧回数
takafuminaka
Contributor II

Dear chipexpert ,

Thank you very much for your quick reply.

For supporting this issue, we set CCM_CLPCR[LPM] as 00.

But it doesn't have any impact on this issue.

Is there any other registers for using "Remain in run mode" setting?

0 件の賞賛
939件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

This has not relation to low power modes.

During VSYNC,HSYNC i.MX6 does not fetch data

from memory, so there may be no DDR clock during LCD synch pulses.

Best regards

chip

0 件の賞賛