iMX6L lack of DDR clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6L lack of DDR clock

Jump to solution
1,054 Views
takafuminaka
Contributor II

Hello,

We observed the lack of DDR base clock.

The clock periodically stops( 0V ).

It seems the cycle is in synchronization with LCD display's VSYNC and HSYNC.

We attached the waveform.

Could you let us know the reason about this issue?

Is this normal behavior?

Thank you.

Labels (2)
Tags (1)
0 Kudos
1 Solution
924 Views
igorpadykov
NXP Employee
NXP Employee

This has not relation to low power modes.

During VSYNC,HSYNC i.MX6 does not fetch data

from memory, so there may be no DDR clock during LCD synch pulses.

Best regards

chip

View solution in original post

0 Kudos
3 Replies
924 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takafumi

if customer does not have other issues (such as OS hanging

ot other misbehaviour), then this seems as normal

behaviour. Becasue during VSYNC,HSYNC i.MX6 does not fetch data

from memory, so there may be no DDR clock during LCD synch pulses.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
924 Views
takafuminaka
Contributor II

Dear chipexpert ,

Thank you very much for your quick reply.

For supporting this issue, we set CCM_CLPCR[LPM] as 00.

But it doesn't have any impact on this issue.

Is there any other registers for using "Remain in run mode" setting?

0 Kudos
925 Views
igorpadykov
NXP Employee
NXP Employee

This has not relation to low power modes.

During VSYNC,HSYNC i.MX6 does not fetch data

from memory, so there may be no DDR clock during LCD synch pulses.

Best regards

chip

0 Kudos