Does i.MX6DL have limitation of giga ethernet?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does i.MX6DL have limitation of giga ethernet?

跳至解决方案
1,009 次查看
JHY
Contributor IV

I use i.MX6DL and RTL8111F(pci ethernet).

When I run iperf in normal status, TX speed is about 600MBits/sec and somtimes disconnection occurs.

But when reducing TX speed to under 300MBits/sec (by adjusting MTU to under 500 or Number of Tx descriptor registers to under 128), there is no disconnetion.

So I want to know whether i.MX6 has a limitation of giga ethernet or not.

If not, advise to me about abobe please.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
812 次查看
igorpadykov
NXP Employee
NXP Employee

Hi conan

there is ERR004512 IMX6SDLCE.

i.MX6 has not other limitations of giga ethernet, as you described.

Issues which you are observing, probably related to RTL8111 settings

and local network configuration. You can consult with local network administrator.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
813 次查看
igorpadykov
NXP Employee
NXP Employee

Hi conan

there is ERR004512 IMX6SDLCE.

i.MX6 has not other limitations of giga ethernet, as you described.

Issues which you are observing, probably related to RTL8111 settings

and local network configuration. You can consult with local network administrator.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复