Hi,
We are working on porting Windows 10 IOT to iMX6DL processor. We needs to modify some of the pin mux configurations from default.
1.Should I modify in UBoot alone is enough or I needs to change it in ACPI tables?
2. If I needs to modify in ACPI tables also means, how does it will be built?
3. Debug UART is not giving logs, how to enable that? After some initial boot, it stuck at
#KDTARGET: Refreshing KD connection
ªE/LD: init_elf:238 sys_open_ta_bin(2d57c0f7-bddf-48ea-832f-d84a1a219301)
E/TC:? 0 init_with_ldelf:279 ldelf failed with res: 0xffff0000
E/TC:? 0 tee_ta_open_session:725 Failed. Return error 0xffff0000
Hi @m_syed_ahmed,
The only Windows 10 IOT that we support can be found on the link below:
So for porting this, we do not supported.
Regards,
Israel.
Hi Israel,
We are using iMX6DL processor based custom board. I needs to modify some pin mux from default reference board. Can you help me where to change for pin mux?