iMX6DL Windows 10 IOT Pin Muxing and Debug Port Enabling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6DL Windows 10 IOT Pin Muxing and Debug Port Enabling

830 Views
m_syed_ahmed
Contributor III

Hi,

We are working on porting Windows 10 IOT to iMX6DL processor. We needs to modify some of the pin mux configurations from default.

1.Should I modify in UBoot alone is enough or I needs to change it in ACPI tables?

2. If I needs to modify in ACPI tables also means, how does it will be built?

3. Debug UART is not giving logs, how to enable that? After some initial boot, it stuck at 

#KDTARGET: Refreshing KD connection
ªE/LD: init_elf:238 sys_open_ta_bin(2d57c0f7-bddf-48ea-832f-d84a1a219301)
E/TC:? 0 init_with_ldelf:279 ldelf failed with res: 0xffff0000
E/TC:? 0 tee_ta_open_session:725 Failed. Return error 0xffff0000

0 Kudos
Reply
2 Replies

798 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi @m_syed_ahmed,

 

The only Windows 10 IOT that we support can be found on the link below:

https://www.nxp.com/design/software/embedded-software/i-mx-software/windows-10-iot-core-for-i-mx-app...

 

So for porting this, we do not supported.

 

Regards,

Israel.

0 Kudos
Reply

792 Views
m_syed_ahmed
Contributor III

Hi Israel,

We are using iMX6DL processor based custom board. I needs to modify some pin mux from default reference board. Can you help me where to change for pin mux?

0 Kudos
Reply