Hi all
I get package gpu-viv-bin-mx6q-3.10.17-1.0.0-beta-hfp.bin from Freescale · GitHub yocto project
And make my own buildroot system from liyaoshi/buildroot · GitHub
I have made it run under a custom iMX6 solo board
I can run weston and weston-flower ,weston-terminal on my board now , But
When I try to get weston simple egl demo run on my board . I get Segmentation fault
My question ,
Do gpu-viv-bin-mx6q-3.10.17-1.0.0-beta-hfp.bin this package only support iMX6D and iMX6Q that with VIVANTE gc2000 core ?
If yes .
Do you have package driver for iMX6 Dual lite and solo that with gc880 core ? where can I get it ?
Thanks and regards
Xiongwei
已解决! 转到解答。
Update information
Today I try to use kernel from 3.10.17 ,and seems this will be the right way
current Kernel 3.10,31 from freescale git is NOT compatible with gpu-viv-bin-mx6q-3.10.17-1.0.0-hfp.bin
So ,this might be the conclusion.
I will use 3.10.17 GA kernel
BTW ,Do FSL have plan update GPU driver to support newer version ?
The /dev/galcore driver in Linux 3.14 expects a driver argument like the following for the IOCTL_GCHAL_INTERFACE ioctl.
typedef struct _DRIVER_ARGS
{
gctUINT64 InputBuffer;
gctUINT64 InputBufferSize;
gctUINT64 OutputBuffer;
gctUINT64 OutputBufferSize;
}
DRIVER_ARGS;
Each InputBuffer and OutBuffer must be a gcsHAL_INTERFACE type which currently has a size of 248 bytes. To verify what the current iMX6Q libGAL.so is passing to the kernel I set a breakpoint on the first call to ioctl() when querying the interface parameters. On inspecting the $r2 ioctl argument, the current iMX6Q GPU drivers are passing a DRIVER_ARGS which contains 32-bit values, not the gcfUINT64 values expected by the 3.14 kernel. In addition, the size of the gcsHAL_INTERFACE parameters was apparently 128 bytes at the time the iMX6Q GPU driver was compiled.
(gdb) info registers
r0 0xffffffe7 4294967271
r1 0x7530 30000
r2 0x7efef7fc 2130638844
r3 0x14008 81928
r4 0x76fb9ee8 1996201704
r5 0x7530 30000
r6 0x2710 10000
r7 0x80 128
r8 0x7efef838 2130638904
r9 0x1 1
r10 0xaaa22a22 2862754338
r11 0xffffffff 4294967295
r12 0x76fb692c 1996187948
sp 0x7efef7f0 0x7efef7f0
lr 0x76fa7fec 1996128236
pc 0x76eb0bec 0x76eb0bec <ioctl+12>
cpsr 0x200e0030 537788464
(gdb) x/8x $r2
0x7efef7fc: 0x7efef838 0x00000080 0x7efef838 0x00000080
0x7efef80c: 0x00024078 0x00022930 0x00000000 0x0002407c
Please, Freescale could you rebuild these drivers to support the current 3.14 kernel!
Regards,
Jonathan
Update information
Today I try to use kernel from 3.10.17 ,and seems this will be the right way
current Kernel 3.10,31 from freescale git is NOT compatible with gpu-viv-bin-mx6q-3.10.17-1.0.0-hfp.bin
So ,this might be the conclusion.
I will use 3.10.17 GA kernel
BTW ,Do FSL have plan update GPU driver to support newer version ?
Hi all
update information
When I use weston with EGL I get error
And from strace log
open("/dev/fb0", O_RDWR) = 12
ioctl(12, FBIOGET_VSCREENINFO, 0xa57624) = 0
ioctl(12, FBIOGET_CONTRAST or FBIOPUT_VSCREENINFO, 0xa57624) = 0
ioctl(12, FBIOGET_VSCREENINFO, 0xa57624) = 0
ioctl(12, FBIOGET_FSCREENINFO or FBIOPUT_CONTRAST, 0xa575e0) = 0
mmap2(NULL, 1536000, PROT_READ|PROT_WRITE, MAP_SHARED, 12, 0) = 0x7698f000
rt_sigaction(SIGFPE, NULL, {SIG_DFL, [], 0}, 8) = 0
rt_sigaction(SIGFPE, {0x76f24d0c, [], SA_RESTART|SA_SIGINFO|0x4000000}, NULL, 8) = 0
futex(0x76f4e424, FUTEX_WAKE_PRIVATE, 2147483647) = 0
open("/dev/galcore", O_RDWR) = 13
ioctl(13, 0x7530, 0x7e954628) = -1 ENOTTY (Inappropriate ioctl for device)
ioctl(13, 0x7530, 0x7e954600) = -1 ENOTTY (Inappropriate ioctl for device)
--- SIGSEGV {si_signo=SIGSEGV, si_code=SEGV_MAPERR, si_addr=0xd4} ---
+++ killed by SIGSEGV +++
Segmentation fault
#
I get gpu package from http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/gpu-viv-bin-mx6q-3.10.17-1.0.0-hfp.bin and kernel based on freescale git tree of branch remotes/origin/imx_3.10.31_1.1.0_alpha
Any help would be appreciate
Regards
update information
I test same code on iMX6Q with gc2000 core ,and for more simply case, I use libEGL-fb.so and test with vv_launcher
but unfortunately I got same code error
strace log shows the ioctl error
open("/usr/lib/libEGL.so", O_RDONLY|O_CLOEXEC) = 3
read(3, "\177ELF\1\1\1\0\0\0\0\0\0\0\0\0\3\0(\0\1\0\0\0D)\0\0004\0\0\0"..., 512) = 512
fstat64(3, {st_mode=S_IFREG|0755, st_size=379514, ...}) = 0
close(3) = 0
munmap(0x76fce000, 18206) = 0
rt_sigaction(SIGINT, {0x76ef046c, [], SA_INTERRUPT|SA_NODEFER|SA_RESETHAND|0x4000000}, {SIG_DFL, [], 0}, 8) = 0
rt_sigaction(SIGQUIT, {0x76ef046c, [], SA_INTERRUPT|SA_NODEFER|SA_RESETHAND|0x4000000}, {SIG_DFL, [], 0}, 8) = 0
rt_sigaction(SIGTERM, {0x76ef046c, [], SA_INTERRUPT|SA_NODEFER|SA_RESETHAND|0x4000000}, {SIG_DFL, [], 0}, 8) = 0
open("/dev/fb0", O_RDWR) = 3
ioctl(3, FBIOGET_VSCREENINFO, 0x41a1cc) = 0
ioctl(3, FBIOGET_CONTRAST or FBIOPUT_VSCREENINFO, 0x41a1cc) = 0
ioctl(3, FBIOGET_VSCREENINFO, 0x41a1cc) = 0
ioctl(3, FBIOGET_FSCREENINFO or FBIOPUT_CONTRAST, 0x41a188) = 0
mmap2(NULL, 1536000, PROT_READ|PROT_WRITE, MAP_SHARED, 3, 0) = 0x76b75000
rt_sigaction(SIGFPE, NULL, {SIG_DFL, [], 0}, 8) = 0
rt_sigaction(SIGFPE, {0x76eec854, [], SA_RESTART|SA_SIGINFO|0x4000000}, NULL, 8) = 0
futex(0x76f1568c, FUTEX_WAKE_PRIVATE, 2147483647) = 0
open("/dev/galcore", O_RDWR) = 4
ioctl(4, 0x7530, 0x7eb6b940) = -1 ENOTTY (Inappropriate ioctl for device)
ioctl(4, 0x7530, 0x7eb6b918) = -1 ENOTTY (Inappropriate ioctl for device)
--- SIGSEGV {si_signo=SIGSEGV, si_code=SEGV_MAPERR, si_addr=0xd4} ---
+++ killed by SIGSEGV +++
Segmentation fault
I use kernel from http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.10.31_1.1.0_alpha
And gpu driver from http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/gpu-viv-bin-mx6q-3.10.17-1.0.0-hfp.bin
Toolchain and libc from http://releases.linaro.org/13.11/components/toolchain/binaries/gcc-linaro-arm-linux-gnueabihf-4.8-20...
Regards
Xiongwei