Hello,
I have a strange error with my custom iMX6 board, running Yocto -> fido | meta-qt5 -> fido.
The framebuffer device comes up and I see picture on my LCD screen, but after some minutes I get the following error:
root@imx6qsabresd:~# imx-ipuv3 2400000.ipu: ch = 9, pm_runtime_put failed:-38!
CPU: 0 PID: 25 Comm: kworker/0:1 Not tainted 3.14.28-1.0.0_ga+g91cf351 #7
Workqueue: events console_callback
[<80014644>] (unwind_backtrace) from [<8001164c>] (show_stack+0x10/0x14)
[<8001164c>] (show_stack) from [<8065485c>] (dump_stack+0x7c/0xbc)
[<8065485c>] (dump_stack) from [<80459cdc>] (ipu_uninit_channel+0x524/0xa7c)
[<80459cdc>] (ipu_uninit_channel) from [<802ca220>] (mxcfb_blank+0x80/0xb8)
[<802ca220>] (mxcfb_blank) from [<802b0550>] (fb_blank+0x54/0xa8)
[<802b0550>] (fb_blank) from [<802ba92c>] (fbcon_blank+0xf4/0x2a8)
[<802ba92c>] (fbcon_blank) from [<802f6604>] (do_blank_screen+0x1d4/0x284)
[<802f6604>] (do_blank_screen) from [<802f94dc>] (console_callback+0x88/0x15c)
[<802f94dc>] (console_callback) from [<8003ed2c>] (process_one_work+0xf4/0x35c)
[<8003ed2c>] (process_one_work) from [<8003f97c>] (worker_thread+0x130/0x3bc)
[<8003f97c>] (worker_thread) from [<80044c3c>] (kthread+0xcc/0xe4)
[<80044c3c>] (kthread) from [<8000e478>] (ret_from_fork+0x14/0x3c)
And my screen goes off (pixel clock stops)
Does anyone have any idea what could be the problem?
Thank you in advance!
Best regards,
Krisztián Bakos
已解决! 转到解答。
Hello Alfred,
Thank you for the answer. The thing is, that the power management was disabled in the Kernel, thus it could not switch power states. I re-enabled it and now it works fine. However, this was not such a huge issue as I could re-enable the screen (turned out it was the "screensaver"... -.-')
Best Regards,
Krisztián
Hello Alfred,
Thank you for the answer. The thing is, that the power management was disabled in the Kernel, thus it could not switch power states. I re-enabled it and now it works fine. However, this was not such a huge issue as I could re-enable the screen (turned out it was the "screensaver"... -.-')
Best Regards,
Krisztián