iMX6 fb1 and fb0 resolutions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 fb1 and fb0 resolutions

2,510件の閲覧回数
alexanderkhudos
Contributor I

In iMX6 fb0 resolution is set to the value specified by videoargs in uboot. fb1 (foreground of the same display) always comes up with the resolution 240x320. Is there a way to set it to the same resolution?

ラベル(4)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

1,315件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can use the tools, for example:

fbset -fb /dev/fb1 -xres * -yres*

0 件の賞賛
返信

1,315件の閲覧回数
alexanderkhudos
Contributor I

I know about fbset. My question was whether it is possible to set it to the same resolution automatically. And why does it always come up with the resolution 240x320?

0 件の賞賛
返信

1,315件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you should change the source code. the framebuffer source code in the bsp, but I don't think you need to do that.

0 件の賞賛
返信

1,315件の閲覧回数
alexanderkhudos
Contributor I

I should not change the source code, driver creators should. Or is it a feature, not a bug that FG and BG screen modes are not matched automatically?

0 件の賞賛
返信

1,315件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I don't think this is a bug

0 件の賞賛
返信