Hello all
I get reading from
Document Number: IMX6DQRM Rev. 1, 04/2013 @ Page 2696
• RGB565 over 16 bit = 2 cycles/pixel
As I understand , RGB565 is take 16bit in ram , and all dma transfer can finished in 1 clock with paral data , Why this takes 2 cycles ?
While At the same page
• RGB888 over 8 bit = 3 cycles/pixel
This is fiexed from Document Number: IMX6DQRM Rev. 0, 11/2012 @Page 2671
This is a little wired , I dont know if your chip will have some special trick for dma transfer ? high dma data transfer limit ?
But at same page
• YUV422 over 16 bit = 1 cycles/pixel
Or , just Document error ?
Regards
已解决! 转到解答。
Yes, this is a misprint : RGB565 over 16 bit requires 1 cycle/pixel
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, this is a misprint : RGB565 over 16 bit requires 1 cycle/pixel
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------