I have a Sabre i.MX6 Solox board. The PCIe bus fails with:
imx6q-pcie 8ffc000.pcie: phy link never came up
imx6q-pcie 8ffc000.pcie: DEBUG_R0: 0x00cb8300, DEBUG_R1: 0x08200000
imx6q-pcie 8ffc000.pcie: failed to initialize host: ret: -22
I have tracked this to pcie-designware.c::dw_pcie_host_init->of_pci_parse_bus_range(np, &pp->busn);
This function of_pci_parse_bus_range is looking for the "bus-range" property. I assume that property is coming from one of the DTS files. This version is comprised of 3 DTS included to create the one being used, imx6sx-sdb.dts. None of the DTS files have any "bus-range". I'm wondering if the "ranges" would from imx6sx.dtsi would work. Maybe the property name is justed spelled wrong, again?
If anyone has any ideas about why the "bus-range" property can't be found please let me know.
Randy Silagi
解決済! 解決策の投稿を見る。
Hi Randy
one can look at linux/Documentation/devicetree/bindings/pci/designware-pcie.txt
linux-2.6-imx.git - Freescale i.MX Linux Tree
and try to add this property using example
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Randy
one can look at linux/Documentation/devicetree/bindings/pci/designware-pcie.txt
linux-2.6-imx.git - Freescale i.MX Linux Tree
and try to add this property using example
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------