iMX536 ARD (Rev B) Board - VGA / LVDS Display Failed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX536 ARD (Rev B) Board - VGA / LVDS Display Failed.

871 Views
anjalishyju
Contributor III

I flashed the downloaded images of linux for IMX536 ARD (Rev B) board into the MicroSD,  but when boot up and login as root, fail to bring up the X & Matchbox as shown below:


[iMX56 ARD via USB Serial Cable]

===========================================================

root@freescale ~$ uname -a
Linux freescale 2.6.35.3-744-g27fdf7b #1 PREEMPT Tue Jul 5 13:26:21 SGT 2011 armv7l GNU/Linux


root@freescale ~$ startx
_XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6
_XSERVTransOpen: transport open failed for inet6/freescale:0
_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6
(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base
(EE) XKB: No components provided for device Virtual core keyboard

Backtrace (0 deep):

Fatal server error:
Segmentation fault caught

matchbox-desktop: unable to open display !
matchbox-panel: failed to open displaymatchbox: can't open display! check your DISPLAY variable.
ts_open: No such file or directory

*This iMX53 QSB is tested OK and working fine using the Ubuntu 10.04 (Lucid) MicroSD previously. So its VGA Port, Cable and the LCD Monitor is OK.

* It show same error message even after exporting DISPLAY=:0

0 Kudos
Reply
2 Replies

605 Views
OtavioSalvador
Senior Contributor II

I advise you to test the Yocto Project build as it has several bugfixes included on top of original LTIB BSP.

0 Kudos
Reply

605 Views
SergioSolis
NXP Employee
NXP Employee

Are you using the latest BSP available?

There are a couple of thread that have the same problem as you have, please take a look at them and let me know if you are still experiencing problems...

Re: what is the startx file for imx53 quickstartboard when i addedd the startx file am able to get t...

FSL gnome release package and VGA display output ?

0 Kudos
Reply