iMX535 Fuse Programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX535 Fuse Programming

Jump to solution
812 Views
sherry_zahid
Contributor III

Hi,

I wanted to know how fuse programming works on the iMX535 (using the "fuse" command in u-boot). Are my following assumptions correct:-

1. If fuse bit(s) are not blown the default value = 0 

2. fuse bit is only blown once you program a value of 1 (and the configuration/fuse retains this value permanently)

I was unable to find this exact information in the ref manual / datasheet.

Thanks
SZ

Labels (2)
Tags (3)
1 Solution
712 Views
igorpadykov
NXP Employee
NXP Employee

Hi sherry

1. right

2. right

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
713 Views
igorpadykov
NXP Employee
NXP Employee

Hi sherry

1. right

2. right

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------