iMX287 can't reset by RESETN pin.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX287 can't reset by RESETN pin.

1,182 次查看
f43067
Contributor II

Hello everybody:

    In my project I use iMX287 as the MCU, and an external watchdog chip connected to the RESETN pin of the iMX287, but I found sometimes the RESETN pin can't reset the iMX287 successfully, and in this condition the iMX287 will continuously ‘died’ until turn off the 5V power and turn on it. In this 'died' condition, I found the VDDIO drop down to 3.1~3.2V, VDDD drop down to 1.2V and VDDA drop down to 1.0~1.1V. This happened immediately when the RESETN drop down to 0V. I use the official power_prep.c and patch it by L2.6.35_10.12_SDK_5V_SUPPLY_PATCH.

    I don't know why this happened, and I also don't know in which condition this will happen. How can I solve this problem?

    Best regards. 

1 回复

930 次查看
art
NXP Employee
NXP Employee

As far as I understand, you use the 5V only power scheme. So, please refer to the attached document, especially, to its Section 3.1.2 "VDD5V source only", for all 5V only power related hardware and software considerations.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复