iMX283 : VDDD is connected to DCDC_VDDD directly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX283 : VDDD is connected to DCDC_VDDD directly

Jump to solution
933 Views
koichisakagami
Contributor II

Dear community,

We are designing a custom board.

[Background]
We are referring the schematic of MX28EVK.
The DCDC_VDDD output  is directly inputted into VDDD0-6 .
We know that theDCDC_VDDD should not exceed 1.55V taking into account +3 %
tolerance (when DCDC_VDDD is used to power the VDDD).
We have to drop a DCDC_VDDD voltage for the VDDD margin.

[Question]
What is the recommended solution to drop the DCDC_VDDD voltage ?
Should we insert a resistance or a diode ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
839 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
2 Replies
840 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
839 Views
Yuri
NXP Employee
NXP Employee

  The DC-DC converters include such feature as programmable output voltages.
This allows to setup the needed voltage level. Please refer to app note AN4199
for some details how to treat with i.MX28 Power Management Unit.

http://cache.freescale.com/files/32bit/doc/app_note/AN4199.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos