iMX28 with WINCE6 Nand boot - power supply volages error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28 with WINCE6 Nand boot - power supply volages error

695 Views
shany
Contributor II

Hello,

I'm working on an application based on  iMX283.

I have the  evk as a reference board +  my own design. I'm trying to load eboot image using the sb_loader program.

The evk works fine, but I have a problem with my application.

The processor is connected to both    5V + battery.

The measured voltages are - VDDIO = 3.3V, VDDA =  1.8V, VDDD = 1.2V.

I've done a little research and found that the process fails in the BootFromBattery() function - where the DCDC is supposed to be enabled - this is the line (In the xldr.c)   -

 

//Enable DCDC

HW_POWER_5VCTRL_SET(BM_POWER_5VCTRL_ENABLE_DCDC).

When trying to load eboot to my application – the process fails and the processor SHUTS DOWN when coming to Enable DCDC.

Running it with the DCDC Disabled – comes out OK.

 

Does anyone have an idea or suggestions for additional tests?  

Thanks in advance,

Shany 

0 Kudos
Reply
1 Reply

557 Views
admin
Specialist II

Hi,

Just wondering if this was resolved as I'm facing the same issue.

Thanks,

Pat

0 Kudos
Reply